Code Verification
111 topics in this forum
-
- 1 reply
- 169 views
The LVS-95XX software supports printing functions in several areas, but the software itself does not let you choose a destination printer. Rather, the LVS-95XX uses the default Windows printer. Supported Devices: · All LVS-95XX devices utilizing LVS-95XX software. Instructions: 1. Before selecting the desired Windows default printer, ensure the LVS-95XX software is closed since any changes made won’t take effect until the software is restarted. 2. In Windows, navigate to the “Control Panel” > “Devices and Printers”. 3. Locate the printer to be the Windows default, right-click on its icon, then in t…
Last reply by Damian, -
On rare occasions, the error below may appear when using an LVS-95XX-series barcode verifier: “Warning: A camera contains a non-numeric serial number and cannot be accessed”. A similar and related error message may appear which includes the phrase “DEADBEEF”. Unlike other potential error messages that may make mention of the verifier’s serial number, both of these error messages indicate an unrecoverable camera hardware failure. If you encounter either of these errors, please contact OMRON Technical Support through a channel below to explore possible factory repair options or to be put in touch with a sales representative for a quote to purchase a replacem…
Last reply by Troy Shaw, -
This error message indicates that the .mdb file has reached or surpassed the 2GB size limit (dictated by the MS Access size limit). The resolution for this is to first run C:\Program Files (x86)\\Microscan\LVS-95XX\CompactLvsDb.exe to compact the .mdb file below the size limit, then create a backup database using the Archive tab in LVS-95XX and then deleting a sufficient number of reports to get well under the size limit. See page 92 of the operator manual for further details on database backup. Operating System Any
Last reply by Omron Forums Support, -
Due to changes made to the ISO 15416 verification standard in December 2017, letter grades are no longer displayed for overall symbol grades in LVS-95XX software version 4.3.0.3006 and later. Attached is a technical note outlining the changes to the standard and the LVS-95XX software. Software Version 4.3.0.3006 Operating System Any kA23800000008RYCAY_en_US_1.pdf
Last reply by Omron Forums Support, -
LVS-95XX software most closely aligns with a GAMP 4 (Configurable Software Packages) category.
Last reply by Omron Forums Support, -
- 0 replies
- 193 views
p by step procedure demonstrating how to use the PDF comparator in the LVS75xx application. Overview The comparison of the LVS-7510 golden to the Master PDF file happens only at setup.ScanProof compares the .BMP version of the LVS-75XX golden image created from the label during the AutoSetup process to a PDF Master artwork file selected by the user.This comparison happens on only one image; the golden image taken during setup. After the comparison in ScanProof, the LVS golden image is compared to the image of every label printed. Operation From the Blemish setup screen of the LVS-75XX software, the Correlate Artwork button launches the ScanProof application. The LVS…
Last reply by Omron Forums Support, -
- 0 replies
- 116 views
This is usually caused by the customer changing settings in the INI file under [Camera]. They put Flip=1. This tried to reverse the pixel readout, but flip only ever worked for a specific camera: Dalsa P2-4x-04K40. When this setting was changed in the INI file it reversed the tap readout. This caused vertical blank lines in the image. The symptoms looked exactly like another issue that was related to a known Basler Power Supply issue. Once Flip=0 was reset, the image was fine, however the image was now mirrored. This explains why Flip= was changed to try to deal with the mirrored image. The actual fix is to rotate the camera 180. In this particular case, the entire 7000 …
Last reply by Omron Forums Support, -
- 0 replies
- 132 views
To view the licenses enabled the system, make sure the dongle is connected to the PC and start the 7XXX software. Before logging into the software press CTRL-A and a window will be displayed showing the current licenses. The attached files shows how this looks with 7000 software.
Last reply by Omron Forums Support, -
- 0 replies
- 149 views
When this warning is shown at the bottom of the MICROSCAN LVS© Grading tab, yet the code is receiving an A grade, it is notifying the User that there is an unprintable character in the embedded data string. While not a failure, we do notify that the unprintable character is present. Review Unprintable Characters on Structure Tab In this example, when directed to the Structure tab, the data structure analysis is viewable. In this string of data, there is a <Space>. A space cannot be printed, but is present in the data. Software Version LVS-95XX Firmware Version LVS-95XX Operating System Any
Last reply by Omron Forums Support, -
- 0 replies
- 97 views
The use of the "Import image from file" function via the Archive tab of LVS-95XX software is not possible with DPM standards such as ISO/IEC TR29158. The process of grading a DPM symbol requires using a live image. Only with this live image can TR29158 rules can be applied. Software Version All Operating System Windows 10;Windows 7;Windows XP
Last reply by Omron Forums Support, -
- 0 replies
- 138 views
Most mid and high range label design software allows for re-scaling of print templates for different dpi of printers. In that case a customer who has designed print templates for a 203 dpi printer and would like to purchase a LVS-7510 with 300 dpi printer can easily adjust their print templates for use with the LVS-7510 system. For customers using label design software that does not provide this easy re-scaling, it would be required to create new print templates. A 203 dpi version of the ZT600 series will be supported by LVS-7510 in 2018. However, it is recommended that only barcodes with x-dimensions of 15 mil or larger be used with that resolution printer to help mi…
Last reply by Omron Forums Support, -
- 0 replies
- 119 views
Due to camera drivers used on older (2013 and earlier) models of LVS-9510 and LVS-9570, version 4.3 software released in December 2017 is not supported for these older units. LVS-9570 with a serial # that is lower than 14140 (December 2013 and older) cannot be upgraded. LVS-9510 with serial #s 12906 and lower (prior to June 15, 2012) also are not compatible with version 4.3 and later software. Software Version 4.3 and newer Operating System Windows 10;Windows 7;Windows XP
Last reply by Omron Forums Support, -
- 0 replies
- 110 views
Since both Win 7 and Win 10 were released after the UID Checker, we have not retested the software using those OS versions. However, we have many customers using Win 7 and Win 10 successfully and I have not heard of anyone trying to install the software on Win 8 yet. Operating System Windows 7
Last reply by Omron Forums Support, -
- 0 replies
- 126 views
Over the years, operational requirements of GS1 System users have influenced the dimensional specifications of GS1 System symbols, and these dimensional specifications have in turn influenced the development of scanning system optics and printing processes. The dimensional requirements for each application area defined in Section 2 of General Specifications are set out in the GS1 System Symbol Specification Tables (SSTs). In the previous version of software, there was greater symmetry in the chosen aperture. With version 15, there have been changes to the required aperture for EAN/UPC-A (Table 2 now requires a 10 mil aperture where previously it was 6 mil), GS1 Data Mat…
Last reply by Omron Forums Support, -
- 0 replies
- 73 views
If scanning the RIMS barcode, but file is not found: Insure the QC or LVS7000 PC is turned ON. RIMS can only retrieve job data from a powered PC. Insure the QC / LVS7000 PC is on the Network. This may require customer IT support. Insure the JOBS folder on the In1= PATH (QC / LVS7000 PC) has File Sharing enabled. This may require customer IT support. [Rims] A5Follows=4 Debug=0 EncoderDirection=0 EncoderPort=5 HomeToPhotoeye=12 In1=\\Server1\PathToJobsDir In2=\\Server2\PathToJobsDir In3=\\Server3\PathToJobsDir Out=\\ServerX\PathToJobsDir LinesPerInch=400 MoveBarcodeInches=0 RewinderOffset=41500 StopDwellInMs=20 Turret=0 Insure the RIM system currently logged in Windows Use…
Last reply by Omron Forums Support, -
- 0 replies
- 118 views
The LVS-9570 operator manual describes the proper technique for verifying a barcode when using LVS-9570. The unit should be pulled at a slow, steady rate toward the user in the direction toward the back of the unit (where the USB connector is located). This is in the opposite direction of the arrow printed on the outside of the housing, which is used to indicate where the center of the scanning sensor is located. If the LVS-9570 is pulled too quickly across the label, then an over-speed error will be displayed in the LVS-95XX software and no grade will be provided. Barcodes of up to 305 mm (12") long can be scanned in a ladder orientation, with a maximum 137mm (5.4") …
Last reply by Omron Forums Support, -
- 0 replies
- 114 views
Follow the link below and use instructions according to your O.S. level. https://help.aol.com/articles/manually-reset-your-internet-protocol-tcp-ip-settings Operating System Any
Last reply by Omron Forums Support, -
- 0 replies
- 127 views
When using the QC "Operator.exe" program, the resulting "Operator.dat" file is saved to the "LVS QC" installation directory. This "Operator.dat" file will need to be copied to the "LVS QC" user area in order for any changes to apply. It can also be copied to the "LVS 7000" and "LVS RIMS" user areas for consistency. Software Version any Operating System Windows 7;Windows XP
Last reply by Omron Forums Support, -
When the LVS-95XX software starts, it tries to determine the database in use (Access, MS SQL, MySQL). It does this by creating a test table and then creating different types of data elements unique to a particular database type. This error can occur if the user name and password in the database connection string contains an expired password, in particular if this is a system that has been working and is now giving this error. They can test this with Windows ODBC admin tool by creating a connection to the database using the SQL server username and password. If the connection fails, then the issue is likely the username and password being expired. If it is successful, the…
Last reply by Omron Forums Support, -
- 0 replies
- 105 views
Last reply by Omron Forums Support, -
- 0 replies
- 163 views
When resetting the password for an Operator ID account in the LVS-95XX software, it is required that you reenter the entire password, rather than simply the characters you are changing. For example, if you are changing the password from "microscan1" to "microscan3", you cannot simply delete the last digit and replace it with "3"; you actually need to delete the entire old password and retype the new password or else the change will not be accepted, producing the below error: Software Version All Operating System Windows 10;Windows 7;Windows XP
Last reply by Omron Forums Support, -
- 0 replies
- 138 views
LVS-7510 Software, OMRON Microscan’s proprietary inline verification and print quality inspection software for use with LVS-7510 for Zebra ZT600 series printers, provides barcode verification and label print quality inspection capabilities. A new camera interface PCB has been released for LVS-9570 and LVS-7510 which requires the use of version v. 20.2.1.4001 for LVS-7510 and software version 4.4.0.4012 or newer for LVS-9570. Software version 20.2.1.4001 software will begin shipping with all new LVS-7510 systems built at OMRON Microscan after May 24, 2018. The spare part LVS-7510 camera driver PCB kit, 98-9000092-01, will be revised to a new revision of PCB which require…
Last reply by Omron Forums Support, -
Make sure that you have administrator privileges to the computer prior to install. 1. Close the LVS-95XX software. 2. Unplug the USB cable of the Microscan system from the computer. 3. Go to Installation Flash Drive > “Other setup” folder > click “Keysetup.exe.” 4. Select “Keylok 2 (USB w/ Driver)” and “Standalone.” 5. Click the “Begin Install” button. A message appears indicating that all files have been copied. Close the dialog box. 6. Plug in the USB cable. 7. Windows should report a "New hardware found” message. Select “No, not this time.” 8. On the next screen, select “Install software automatically.” 9. Click “Finish.” 10. Run the LVS-95XX soft…
Last reply by Omron Forums Support, -
- 0 replies
- 125 views
The solution to this issue is that the end user needs to Re-Install and Launch the software for the first time with Full Administrator rights to the PC. It then creates a everyone group so any user can run the software with a User Account Login. Note: Please temporarily turn off all anti-virus software to prevent interference with the LVS-95XX software installation. Error Screenshot: Follow the steps below to reinstall the software. Purpose: Completely uninstall and re-install the LVS-95XX software. Explanation: In certain situations, it may be necessary to thoroughly and completely uninstall the LVS-95XX software and any residual settings in order to resolve a g…
Last reply by Omron Forums Support, -
- 0 replies
- 101 views
Customer wants to know the maximum number of codes that can be checked for Duplicates The 7000, 75xx software uses an access database when performing duplicate checking. The maximum size of this database is 2 GB. Record size = Data Length + 10 chars (approx) Max # records (approx) = 2,000,000,000 / Record Size INTERNAL NOTE Duplicate checking is performed by attempting to add a record for the current read string to the database. If an error occurs, then the string must already exist and this is a duplicate error.
Last reply by Omron Forums Support,