Jump to content
OMRON Forums

Install a LVS-9510 with a LVS-958X or LVS-9570 System


Recommended Posts

Purpose:
This guide will show you how to install a second LVS device on the same PC. In the latest
version of the LVS software, this addition is limited to only being able to add an LVS-9510 to a
new or existing install of an LVS-9580-85 or LVS-9570 system.
Explanation:
Under normal circumstances, only one LVS-95XX device can be installed on a single PC. The
reason this is the case is that the LVS software needs a database file with the necessary factory
calibration information. The database files are unique to each device and the LVS-95XX
software can only connect to one database file at a time. This guide will show you how you
can add a device to the LVS software and database file to allow you to add an LVS-9510 to an
LVS-958x or LVS-9570 system.
Supported Devices:
LVS-95XX Software
LVS-9510
LVS-9570
LVS-9580
LVS-9585
What you will need:
[LVS-95XX software install files.
The LVS devices (LVS-9510, LVS-9510 etc. .. )
The LVS POTO (PASSWORD OF THE DAY) login credentials

Instructions: 

[PLEASE SEE ATTACHMENT]

LVS-95XX - Install LVS-9510 with an LVS-958X or LVS-9570 System.pdf

Link to comment
Share on other sites

  • Replies 0
  • Created
  • Last Reply

Top Posters In This Topic

Popular Days

Top Posters In This Topic

Popular Days

Join the conversation

You can post now and register later. If you have an account, sign in now to post with your account.

Guest
Reply to this topic...

×   Pasted as rich text.   Paste as plain text instead

  Only 75 emoji are allowed.

×   Your link has been automatically embedded.   Display as a link instead

×   Your previous content has been restored.   Clear editor

×   You cannot paste images directly. Upload or insert images from URL.


×
×
  • Create New...