Jump to content
OMRON Forums

ID-40 and MV-40 External Sensor Triggering


Recommended Posts

ID-40 External Sensor Triggering
You first need to have Input Common connected to either the 24V+ pin or Ground pin on the ID-40. Once that is done the Trigger pin will need to receive the opposite signal of whatever is connected to Input Common. So if Input Common is connected to the 24V+ pin on the ID-40, the Trigger pin would need to be pulled to Ground, and vice versa.


MV-40 External Sensor Triggering
To trigger the MV-40, first make sure that the active vision job file loaded on the camera has the trigger set to "Sensor" so that it is actually expecting a hardware trigger signal on that trigger pin. Then when it comes to wiring, you first need to have Input Common connected to either the 24V+ pin or Ground pin on the MV-40. Once that is done the Trigger pin will need to receive the opposite signal of whatever is connected to Input Common. So if Input Common is connected to the 24V+ pin on the MV-40, the Trigger pin would need to be pulled to Ground, and vice versa.

image.thumb.png.37454639499975cac46d7525628dfc7b.png

image.png.409cbee051292d2d699ae30bc5e9bbbd.png

image.png.186b2b61c984117064580e87c71ac24b.png

Link to comment
Share on other sites

  • Replies 0
  • Created
  • Last Reply

Top Posters In This Topic

Popular Days

Top Posters In This Topic

Popular Days

Posted Images

Join the conversation

You can post now and register later. If you have an account, sign in now to post with your account.

Guest
Reply to this topic...

×   Pasted as rich text.   Paste as plain text instead

  Only 75 emoji are allowed.

×   Your link has been automatically embedded.   Display as a link instead

×   Your previous content has been restored.   Clear editor

×   You cannot paste images directly. Upload or insert images from URL.


×
×
  • Create New...