Jump to content
OMRON Forums

"The Required FNC1 Was Not Found" Error


Recommended Posts

<FNC1> is a "non-printable" special character reserved for GS1-compliant symbols when using Code 128, QR code or Data Matrix symbologies. It is what indicates that a symbol is a GS1-128 symbol, for example, rather than just a regular Code 128. If “GS1 General Specifications” is selected as the Application Standard on the “Setup” tab, and <FNC1> is not encoded in the first position of the code, the code will automatically be graded an “F” since it is not GS1 compliant (see bottom image). If the code is intended to be GS1 compliant, notify the originator that GS1 requires <FNC1> to be present at the start of the symbol. If you are not grading a GS1 barcode, change your Application Standard on the “Setup” tab to “ISO/IEC 15415/15416” or other appropriate Application Standard.

User-added image

Software Version

All

Firmware Version

All

Operating System

Any

Link to comment
Share on other sites

  • Replies 0
  • Created
  • Last Reply

Top Posters In This Topic

Popular Days

Top Posters In This Topic

Join the conversation

You can post now and register later. If you have an account, sign in now to post with your account.

Guest
Reply to this topic...

×   Pasted as rich text.   Paste as plain text instead

  Only 75 emoji are allowed.

×   Your link has been automatically embedded.   Display as a link instead

×   Your previous content has been restored.   Clear editor

×   You cannot paste images directly. Upload or insert images from URL.


×
×
  • Create New...