Omron Forums Support Posted March 14, 2022 Share Posted March 14, 2022 Many PCs have multiple network adapters, like a wireless and wired network adapter. If multiple network adapters are accessing the same subnet that contains the Microscan smart camera Windows does not know which physical adapter to use and causes the software to stop responding. The most frequent cause of this problem is when one network adapter is configured to DHCP and the DHCP server assigns an IP address in the same range. To the user, the software previously worked and now mysteriously doesn't work. To check the network adapter IP address and subnet: Click the Windows Start Button ? All Programs ?Accessories ? click to open a Windows Command Prompt Type the following command in the command prompt window: ipconfigReview the IP address and subnet of each network adapter and confirm that each network is on a unique subnet. If multiple network adapters are on the same subnet, change the TCP/IP v4 properties so that it has a unique subnet.The picture below shows an example of 2 network adapters that are on the same subnet. The IP Address of the red circled item will need to be changed to a unique subnet to correct this problem.Note* All Bold Commands are case Sensitive? Operating System Any Quote Link to comment Share on other sites More sharing options...
Recommended Posts
Top Posters In This Topic
1
Popular Days
Mar 14
1
Top Posters In This Topic
Omron Forums Support 1 post
Popular Days
Mar 14 2022
1 post