Omron Forums Support Posted March 14, 2022 Share Posted March 14, 2022 In order to downgrade a VS-1, you need to do this using HawkEye 1600(T) Firmware Update when Visionscape 4.1.1 (or latest version) was installed. If the VS-1 smart camera has firmware that is newer than the Visionscape version currently in use on the PC the VS-1 downgrade does not work. The instructions below assumes that you have the first version of Visionscape installed on the PC was Visionscape 3.7.2 and that Visionscape 4.1.1 (or latest version) was installed afterward. 1. Install (or Switch) to Visionscape 4.1.1. 2. Run Start menu > Programs > Microscan Visionscape >Tools >HawkEye 1600(T) Firmware Update and select the VS-1 to downgrade. 3. In the Firmware Version dropdown box, select the 3.7.2 firmware. 4. Click update Firmware. 5. When the Firmware update has been completed, close the HawkEye 1600(T) Firmware Update. 6. menu > Programs > Microscan Visionscape >Tools > Visionscape Version Manager to change version to 372_18. Quote Link to comment Share on other sites More sharing options...
Recommended Posts
Top Posters In This Topic
1
Popular Days
Mar 14
1
Top Posters In This Topic
Omron Forums Support 1 post
Popular Days
Mar 14 2022
1 post