Omron Forums Support Posted March 14, 2022 Share Posted March 14, 2022 Each LVS-95xx can be identified via a “reference” name, which could be the unit serial # or factory production area for example.When the data archive is exported to a mapped network folder into a database such as Excel, using a vertical bar field separator, it will include a field that has the reference name for each record in that file.The files can then be manually combined if desired into a single file where the reference field would be used to denote which LVS-95xx that record came from. Quote Link to comment Share on other sites More sharing options...
Recommended Posts
Top Posters In This Topic
1
Popular Days
Mar 14
1
Top Posters In This Topic
Omron Forums Support 1 post
Popular Days
Mar 14 2022
1 post