Omron Forums Support Posted March 14, 2022 Share Posted March 14, 2022 Install the User Mode Process Dumper (userdump) Utility 1. Download the utility User Mode Process Dumper Version 8.1 © Microsoft Corporation. (http://www.microsoft.com/downloads/en/details.aspx?FamilyID=E089CA41-6A87-40C8-BF69-28AC08570B7E&displaylang=en ). 2. Extract the downloaded archive into a folder (C:\kktools\userdump8.1, by default).3. Run setup.exe from the folder: for Windows XP / 2003 32-bit: C:\kktools\userdump8.1\x86.4. In the Setup Wizard, click Next.5. (32-bit OS only) In the Terminate Mode window, select Disable "Dump on Process Termination" feature and click Next . 6. Click Finish and wait for the installation to complete. 7. In the User Mode Process Dump Setup window, click No. Get the Process Dump File 1. Run AutoVISION and reproduce the error.2. When the error has occurred, Open Windows Task Manager (Ctrl-Alt-Del).3. Go to the Processes tab. 4. Go to View -> Select Columns. 5. Check PID (Process Identifier): 6. Next to the Image Name – AutoVISION.exe, you will see PID. 7. Once you have noted down the PID of the process, open Windows Command Line (Start-Run -> cmd) and navigate to the userdump.exe file by issuing the following command: Windows 32 bit: cd /d C:\kktools\userdump8.1\x86 8. Then issue the following command: Userdump xxxx where xxxx is the PID that you have noted down previously. 9. In the C:\kktools\userdump8.1\xxx folder, you will see a PROCCESSNAME.dmp. For example, AutoVISION.dmp.10. Compress the dump file into a ZIP file.11. Upload the dump file to the FTP server. Operating System Windows XP Quote Link to comment Share on other sites More sharing options...
Recommended Posts
Top Posters In This Topic
1
Popular Days
Mar 14
1
Top Posters In This Topic
Omron Forums Support 1 post
Popular Days
Mar 14 2022
1 post