Omron Forums Support Posted March 14, 2022 Share Posted March 14, 2022 Open a Windows Command Prompt from Windows Start Button ? All Programs ? Accessories.At the line prompt Type: telnet XXX.XXX.XXX.XXX (Where "X" is the Ethernet IP address of the connected device)Then login usingVsWorx login: targetPassword: password (you will not see this echoed on the screen)At the "->" prompt type BP_DumpAll + EnterScroll up in the dump list and look for the Power Strobe parameter it should be set to disabled.Scroll Back down to the "->" prompt and type BP_UpdateDevCapsPowerStrobe 1, “MSCANFACTUNLK” + EnterIf entered properly you will see:Writing file to SPI flash...100%value = 0 = 0x0Again at the "->" prompt type BP_DumpAll + EnterScroll up in the dump list and look for the Power Strobe parameter which now shows Enabled.To end the session type: reset + EnterIt displays "Connection to host lost" and unit will reboot.Notes:All Black Bold typed commands are Case Sensitive.All Blue Bold Italicized are replies or generated from the system+ Enter = Hit the Enter Key Operating System Any Quote Link to comment Share on other sites More sharing options...
Recommended Posts
Top Posters In This Topic
1
Popular Days
Mar 14
1
Top Posters In This Topic
Omron Forums Support 1 post
Popular Days
Mar 14 2022
1 post