Omron Forums Support Posted March 14, 2022 Share Posted March 14, 2022 Why we get "Packet Missing from image sent by Camera X" message is that we are out of network resources for the particular NIC port the camera is attached to. The way to reduce network resources are: * Get latest update of the network card device drivers you are using. If the following option(s) are available for your network card device: Increase the # of Receive Descriptors to the maximum Turn Interrupt Moderation On If Jumbo Frames available increase to the maximum number You will also need to update HKLM\Software\Visionscape\GigeVision\PacketSize to the same decimal value so the camera uses that size If those options are not available you will need to Increase the Inter Packet Delay. This will slow the frame rate of the camera since it take longer for an image to transmit from the camera to the PC To Increase Inter Packet Delay you will need to update HKLM\Software\Visionscape\GigeVision\InterPacketDelay value in the registry. You can determine the Inter Pack Delay by using the GigE Vision Control tool and manipulating the Frames per second entry in the Inter Packet Delay dialog. This is found in the Stream Channel Control section Quote Link to comment Share on other sites More sharing options...
Recommended Posts
Top Posters In This Topic
1
Popular Days
Mar 14
1
Top Posters In This Topic
Omron Forums Support 1 post
Popular Days
Mar 14 2022
1 post