Jump to content
OMRON Forums

How To - Install an LVS-9510/9570 & an LVS-9580 on a Single PC


Recommended Posts

Under normal conditions, only one LVS-95XX-series barcode verifier model (9510/9570/9580) of each kind may be used on a single PC at one time. But it is possible for one each of different 95XX models to be installed on a single PC, such as a 9510 and 9580 in the case of this application note. This procedure requires that you log in with the Password Of The Day (POTD), so contact Microscan prior to this procedure to obtain those credentials.

Procedure:

  1. Using the USB drive provided with your 9510 (or 9570), install the LVS-95XX software according to the LVS-95XX Series Software Installation Guide located at the following link: http://files.microscan.com/downloadcenter/LVS-9510_User_Manuals.zip.
  2. Next, using the USB drive provided with your 9580, run “setup.exe”, then once the drivers have been installed, cancel the remainder of the installation, using the screenshots below as a guide:
User-added imageUser-added image
User-added image
User-added image
  1. Plug in the power supply and USB cables for the 9510 (or 9570) FIRST.
  2. Plug in the USB cable of the 9580 to the PC.
  3. Start the LVS-95XX software and log in using the Password Of The Day (contact Microscan for this).
  4. You should now have two cameras listed in the “Setup” tab similar to the below screenshot:
User-added image
  1. Select the 9580 in the “Setup” tab, then navigate to the Calibration tab and click “LVS Calibrate” to perform a calibration by following the prompts (on Step 2 of this process regarding Focus, simply click “OK”).
  2. Your 9580 is now calibrated and both verifiers are ready for use. Simply select the camera you want to use in the “Setup” tab whenever you need to switch.

Software Version

LVS-95XX

Operating System

Any

Link to comment
Share on other sites

  • Replies 0
  • Created
  • Last Reply

Top Posters In This Topic

Popular Days

Top Posters In This Topic

Join the conversation

You can post now and register later. If you have an account, sign in now to post with your account.

Guest
Reply to this topic...

×   Pasted as rich text.   Paste as plain text instead

  Only 75 emoji are allowed.

×   Your link has been automatically embedded.   Display as a link instead

×   Your previous content has been restored.   Clear editor

×   You cannot paste images directly. Upload or insert images from URL.


×
×
  • Create New...