Omron Forums Support Posted March 14, 2022 Share Posted March 14, 2022 Once an Image pre-processing step, Binary Morph for example, has been inserted into the Snapshot, the modified image (output buffer) can be seen when an additional vision tool is inserted into the previous step, in this example the user would insert into the Binary Morph another vision step to use the modified image. The user will also be able to see the effect of the Binary Morph on the image when the child vision step is selected. In addition the effect of the image pre-processing step can be seen if the user double clicks inside of the image pre-processing ROI. To return to the original image the user will need to double click on the image. Quote Link to comment Share on other sites More sharing options...
Recommended Posts
Top Posters In This Topic
1
Popular Days
Mar 14
1
Top Posters In This Topic
Omron Forums Support 1 post
Popular Days
Mar 14 2022
1 post