Omron Forums Support Posted March 14, 2022 Share Posted March 14, 2022 The scanners and imagers with a 5V interface all use the same trigger input scheme. The input is rated for 0-24VDC, which will make it compatible with most sensors. The Trigger input uses a 5V pull-up to hold the line in the High state. To activate the input, pull the trigger pin to zero volts, or use an NPN trigger signal. Wiring diagrams are provided in the Appendix of all User's Manuals. This is identical for Input 1 and the New Master pin Quote Link to comment Share on other sites More sharing options...
Recommended Posts
Top Posters In This Topic
1
Popular Days
Mar 14
1
Top Posters In This Topic
Omron Forums Support 1 post
Popular Days
Mar 14 2022
1 post