Omron Forums Support Posted March 14, 2022 Share Posted March 14, 2022 Customers have successfully used the following procedure:1. Before start the installation, enable the option “Run this program in compatibility mode for Windows 7” in the AutoVISION Software installation file (SetupAutoVISION.exe);2. Proceed with the AutoVISION Software installation.3. Enable the same option in the AutoVISION Software execution file – AutoVISION.exe (installed in the folder C:\Microscan\AutoVision – default path).4. Enable the same option in the Visionscape FrontRunner Software execution file – FrontRunner.exe (installed in the folder C:\Microscan\Vscape\7xx_yy\Dll – default path).**7xx_yy = xx_yy will depend on the AutoVISION installed version. Software Version v 3.0.3/7.0.3 Operating System Windows 10 Quote Link to comment Share on other sites More sharing options...
Recommended Posts
Top Posters In This Topic
1
Popular Days
Mar 14
1
Top Posters In This Topic
Omron Forums Support 1 post
Popular Days
Mar 14 2022
1 post