Omron Forums Support Posted March 14, 2022 Share Posted March 14, 2022 The solution to this issue is that the end user needs to Re-Install and Launch the software for the first time with Full Administrator rights to the PC. It then creates a everyone group so any user can run the software with a User Account Login.Note: Please temporarily turn off all anti-virus software to prevent interference with the LVS-95XX software installation.Error Screenshot:Follow the steps below to reinstall the software. Purpose: Completely uninstall and re-install the LVS-95XX software. Explanation: In certain situations, it may be necessary to thoroughly and completely uninstall the LVS-95XX software and any residual settings in order to resolve a given error or issue. This facilitates the re- installation of the software onto the PC from a completely fresh state, as if it was the first time the software had ever been installed. 1. Begin by uninstalling the LVS-95XX software itself. You can do this by going to Control Panel > Programs and Features, as shown below. Then simply follow the prompts to uninstall.2. Uninstall the accompanying drivers, as shown in the screen below. The process will mirror Step 1.3. You will need to delete the existing registry key. Start the Registry Editor by typing “regedit.exe” into the Windows search box, as shown below. Next, delete the registry key highlighted in the second screenshot at one of the following paths: HKEY_LOCAL_MACHINE > SOFTWARE > Wow6432Node > Microscan > LVS-95XX > Database or HKEY_LOCAL_MACHINE > SOFTWARE > Label Vision Systems > Database.4. All Integra 95XX components should now be uninstalled and the PC should be ready for a new installation. If you have the original CD or USB installation media that came with your verifier, you may now insert it and reinstall the software according to the guidelines specified in the LVS-95XX Series Software Installation Guide.If you have been provided a download link for the software, extract the files, then continue to follow the installation guidelines mentioned previously. 5. Once the software has been successfully reinstalled, copy your .mdb file for you verifier to the new folder location. On your original installation media, in the “LVS-95XX” folder, is a file named “I95xx_yyyyy.mdb”, with “xx” being the rest of the model number of your verifier and “yyyyy” being its serial number. This file should be copied and placed in the appropriate folder listed below and renamed appropriately:If you installed 3.0.9qq or earlier: Move to “C:\Users\Public\I9500”; rename to “I9500.mdb”.If you installed 4.0.0h or later: Move to “C:\Users\Public\LVS-95XX”; rename to“LVS-95XX.mdb”. 6. Once installation is complete, plug in the verifier and attempt to login to the software with the below credentials to confirm that the install was successful:Operator ID: adminPassword: admin Software Version 4.X.Xx Operating System Any Quote Link to comment Share on other sites More sharing options...
Recommended Posts
Top Posters In This Topic
1
Popular Days
Mar 14
1
Top Posters In This Topic
Omron Forums Support 1 post
Popular Days
Mar 14 2022
1 post