Omron Forums Support Posted March 14, 2022 Share Posted March 14, 2022 Connect to the ESP software. Enable Code 39 and send and save to reader. Place 7.5 mil barcode at 10 inches away from reader. Go into the Terminal window and type <K28UNLK,,1> into the terminal’s ‘Send’ bar. When you see:"Focus Setup: Place a .075 label @ 10in. Hit return when ready" come up, hit ENTER. Use the + to focus out and – to focus in. Zero Focus position = nnn 90% 7.5MIL, where nnn = 0 to 255 (the current focus position) When you achieve the high read rate (90% or better), Hit ENTER. The reader will show “Focus Setup Passed” To save the new Zero Focus, type <Zp> in the terminal screen. Quote Link to comment Share on other sites More sharing options...
Recommended Posts
Join the conversation
You can post now and register later. If you have an account, sign in now to post with your account.