Jump to content
OMRON Forums

The operation of Matchcode when using the Master Database


Recommended Posts

Every symbol decoded will run through the database. - If the symbol is in the database, it is a Match. - If the symbol is not in the database, it is a Mismatch. At the end of the read cycle, there is only ONE result, which will be (in the order of priority): - If ANY symbols are not decoded (the number of symbols required is set in the Multisymbol option, under Read Cycle), the read cycle result is Noread. - If ANY symbols do not match the database, the result is Mismatch. - If ALL symbols are decoded, and they are in the database, the result is Match. Each of the three outputs can be programmed for one of these events, and in some cases, a combination of these events. Also note that in most readers, when Matchcode is enabled, there is no more ‘good read’. Settings that say ‘Good Read’ now mean ‘Match’.

Link to comment
Share on other sites

  • Replies 0
  • Created
  • Last Reply

Top Posters In This Topic

Popular Days

Top Posters In This Topic

Join the conversation

You can post now and register later. If you have an account, sign in now to post with your account.

Guest
Reply to this topic...

×   Pasted as rich text.   Paste as plain text instead

  Only 75 emoji are allowed.

×   Your link has been automatically embedded.   Display as a link instead

×   Your previous content has been restored.   Clear editor

×   You cannot paste images directly. Upload or insert images from URL.


×
×
  • Create New...