Jump to content
OMRON Forums

Vision HAWK or Vision MINI won't finish booting


Recommended Posts

The Vision HAWK and Vision MINI will refuse to boot with many of the LED indicator lights remaining on if the following conditions are met: 1) The serial port is set to VxWorks (via the "BP_UpdateConsoleTTY 2" command and 2) The serial port is floating (not connected to anything). The workarounds currently are to either connect the serial port (grounding the Rx and Tx are sufficient or to set the serial port connection to none or VsApp ("BP_UpdateConsoleTTY 0" or "BP_UpdateConsoleTTY 1").

Link to comment
Share on other sites

  • Replies 0
  • Created
  • Last Reply

Top Posters In This Topic

Popular Days

Top Posters In This Topic

Join the conversation

You can post now and register later. If you have an account, sign in now to post with your account.

Guest
Reply to this topic...

×   Pasted as rich text.   Paste as plain text instead

  Only 75 emoji are allowed.

×   Your link has been automatically embedded.   Display as a link instead

×   Your previous content has been restored.   Clear editor

×   You cannot paste images directly. Upload or insert images from URL.


×
×
  • Create New...