cdesilva Posted June 24 Share Posted June 24 I am troubleshooting an issue related to a servo motor which we use to drive a monochromator Bragg axis. At a specific range of the motion, we observe that the x-ray beam jitters possibly due to motor oscillation. The motor is driven by an external amplifier and we use power PMAC for torque control. The motion is typically carried out by executing a motion program. We first observe the issue with our data. Afterwards we jogged the motor in the questionable range and was able to narrow down on the range where we see the oscillation. The x-ray beam stabilize upon killing power to the motor. I am guessing that the motor is trying to correct its position during this range. In any case I want to plot relevant variables by gathering data. I have not used the plotting feature for gathering and also not gathered data before. Need some help for the following #1. Determine which variables to plot #2. What is the procedure for plotting given that I can run a trajectory from EPICS controls to execute the motion program Thank you. Quote Link to comment Share on other sites More sharing options...
cdesilva Posted June 25 Author Share Posted June 25 I found instructions on how to do gathering and plotting using IDE. The issue that I am hitting right now is that I am unable to upload the data. It is taking a long time and I think uploading does not work. Any suggestions on where to look at? Quote Link to comment Share on other sites More sharing options...
Faraday MC - Tony Posted June 27 Share Posted June 27 Check your Windows firewall to make sure that DeltaTauGatherProgram is allowed through. Quote Link to comment Share on other sites More sharing options...
Eric Hotchkiss Posted June 27 Share Posted June 27 I am assuming you are using the IDE plot tool for settings and have it open. What firmware and IDE versions are you using? It's possible they we released far enough apart that gathered data does not upload correctly. There is a legacy mode that might be able to help if the firmware is too old for the IDE. Firmware version is visible in the top bar of the IDE or after the command "vers" is issued in the terminal. IDE version is visible in the top bar. It can also help to Start Gather, Stop Gather, Upload and Plot once manually first if the gather tools is misbehaving. What type of encoder is the motor using? Quadrature? Sinusoidal? Serial? Plotting velocity while moving and checking if Gate3[i].Chan[j].CountError is automatically set true (after manually setting it to 0) can help diagnose encoder issues. Quote Link to comment Share on other sites More sharing options...
cdesilva Posted June 29 Author Share Posted June 29 Thank you for the responses. I need to schedule this work again and will get back here when I have some feedback from my end. Quote Link to comment Share on other sites More sharing options...
cdesilva Posted July 5 Author Share Posted July 5 @Tony I do not see it listed under "Allowed apps" All, I am using IDE version 4.0.3.0 Quote Link to comment Share on other sites More sharing options...
cdesilva Posted July 5 Author Share Posted July 5 @Eric. When I open "Plot" it opens up in Legacy mode. I have also installed version 3.1.4.0 of IDE. I have both versions installed now. I have disabled the firewall from Trend security agent. For both versions with the firewall disabled, I still see the "upload data" taking a long time and not succeeding. Quote Link to comment Share on other sites More sharing options...
Alex Anikstein Posted July 7 Share Posted July 7 What version of firmware is on your system? You can find out by using the "vers" command. Quote Link to comment Share on other sites More sharing options...
cdesilva Posted July 7 Author Share Posted July 7 I installed IDE on another workstation. And it works without any issues. I think there is some issue with my laptop setup. Thank you all for your responses. Quote Link to comment Share on other sites More sharing options...
Recommended Posts
Join the conversation
You can post now and register later. If you have an account, sign in now to post with your account.