sdefisher Posted September 19, 2022 Share Posted September 19, 2022 (edited) I have a macro loop set up. And we're having issues with very short feedback spikes. Sub 100 micro seconds. Very large spikes. Causing following error faults. We have troubleshooted it down the to the macro loop (took a while since it looked like electrical noise). We currently have Encoder Table MaxDelta set to 0 for all axes and the manual recommends against this, Is there an easier calculator for setting this value? We have 24 bit feedback. But the units are in LSB feedback per servo cycle. I need to translate that to counts/second basically. Is there a quick and dirty formula available as I hunt down the servo cycle time? Edited September 19, 2022 by sdefisher Quote Link to comment Share on other sites More sharing options...
steve.milici Posted September 19, 2022 Share Posted September 19, 2022 Set the “MaxDelta” higher than your maximum “expected” counts per servo cycle. Quote Link to comment Share on other sites More sharing options...
sdefisher Posted September 29, 2022 Author Share Posted September 29, 2022 On 9/19/2022 at 7:12 PM, steve.milici said: Set the “MaxDelta” higher than your maximum “expected” counts per servo cycle. I did some step moves at max speed to verify my calculations. Interestingly I had to set the gather mode set to Phase. My velocity seemed to be a bit higher in phase vs servo mode. The velocity would overshoot maximum allowed just long enough to cause the MaxDelta parameter to fault the axis (MaxDelta set too low). Does this make sense? The parameter is working as expected now, but I do the the MaxDelta a bit higher than previously expected due to the velocity going way past the maximum for a very short period of time (200-300 microseconds) , causing the max counts/cycle to go way up as well. Quote Link to comment Share on other sites More sharing options...
steve.milici Posted September 29, 2022 Share Posted September 29, 2022 I would think this is reasonable behavior. Quote Link to comment Share on other sites More sharing options...
Recommended Posts
Join the conversation
You can post now and register later. If you have an account, sign in now to post with your account.