Lobenstein Posted December 9, 2022 Share Posted December 9, 2022 Has anyone ran into the before when trying to open a project? This version of the IDE is the same version the project was created in. Quote Link to comment Share on other sites More sharing options...
steve.milici Posted December 14, 2022 Share Posted December 14, 2022 It is not the PC’s version of the project that has the issue. This would indicate the project in the PMAC has a “ProjectLoadErr”: The Sys.ProjectLoadErr status bit is set to 1 if the processor detects an error in the loading of the user project files into active memory during the power-up/reset process. In this case, the system is put in the factory default configuration. It is 0 if no such error is found at this time. It is bit 3 of 32-bit element Sys.Status. Try opening the project in the IDE with “No Device” to see that this is the case. A typical cause of a “ProjectLoadErr” would be corruption of the project. This could be a transient memory issue. Please contact ODT's direct technical support with your full issue details at: ODT-Support@Omron.com Quote Link to comment Share on other sites More sharing options...
Recommended Posts
Join the conversation
You can post now and register later. If you have an account, sign in now to post with your account.