JTopp Posted January 10 Share Posted January 10 I have code using Coord[X].NCalc and Coord[X].LookaheadFlush to determine when the end of the path is calculated. Using the sys.time I trigger an event a certain amount of time before the machine physically reaches the end of the path. I have used this code before and had no problems however with this machine it fails about 5% of the time. This code is in a realtime routine that runs at a frequency of 2khz. I can't seem to figure out what would cause this to not work sometimes. I attached the motion program. Coord[1].LHSize=2000 Coord[1].LHDistance=200 Coord[1].SegMoveTime=1 LHDtime = 200; if (Coord[1].NCalc == 200 && Coord[1].LookAheadFlush == 1 && ShutoffOS == 0) { segToEnd = Sys.Time; ShutoffOs = 1; } if (ShutoffOS) { vElapTime = Sys.Time - segToEnd; if (vElapTime >= ((LHDtime - ValveOffTime)/1000)) { doValve = 0; ShutoffOS = 0; } } PmacSyntax - Copy.txt Quote Link to comment Share on other sites More sharing options...
steve.milici Posted January 11 Share Posted January 11 I don’t know what “ShutoffOS” refers to but I suspect it makes the event asynchronous to the servo cycle. Even a user servo could miss this from time to time. I would suggest using a synchronous variable assignment statement before the “end of path” of your program. Then put an “extra” DWELL0 after that. The synchronous variable assignment statement calculates an expression value and uses it to assign a value to a variable but delays the assignment until the start of actual execution of the next move commanded from the program. See the “Power PMAC User’s Manual” in the section “Synchronous Variable Value Assignment” for implementation details starting on page 558. Quote Link to comment Share on other sites More sharing options...
JTopp Posted January 16 Author Share Posted January 16 Thank you for your response! We are using the ShutoffOS so ensure that once the end of path is in the lookahead buffer we stop that code from executing. That variable is only set high in the code shown above. We are using the NCalc and LookaheadFlush to determine when the end of the path has been calculated and is in the lookahead buffer. I have been able to figure out that the code with NCalc and Lookahead flush is just not being run sometimes. I am looking into using Synchronous variables but it is difficult in our application because we run a lot of different paths, so it is better for us to use a time based shutoff from the end of the path. Quote Link to comment Share on other sites More sharing options...
JTopp Posted January 24 Author Share Posted January 24 I updated my code to use synchronous variables shown in the attachment. I put one at the beginning of the path, I trigger using this one, and one at the end of the path. I am not seeing the same problem as I was, but I am seeing a problem with the trigger happening too late sometimes (about 5% of the time). I put a timer on for the path time, using the two synchronous variables I added, and I found that the times we are turning off too late the path time is shorter by about 15ms. It appears that sometimes the path is running faster. I thought maybe we were exiting the motion program early, but the entire path is being completed. PmacSyntax.txt Quote Link to comment Share on other sites More sharing options...
steve.milici Posted January 25 Share Posted January 25 When the next move after the assignment executes, the value is assigned to the variable. This assignment is done at the real-time interrupt (RTI) priority level. For segmented moves (as in a circle move), the assignment is done at the beginning of the first segment to start within the new programmed move. This could differ by one RTI (or segmentation) cycle from time to time. Since I don’t think you have your RTI period set that long (15ms) I might suspect this time difference is due to how you are triggering from it or your Coord[x].SegMoveTime is “large”. The same program would not have different execution times if the moves have not changed. What is your servo frequency, Sys.RtIntPeriod and Coord[x].SegMoveTime Quote Link to comment Share on other sites More sharing options...
JTopp Posted January 26 Author Share Posted January 26 My servo frequency is set to 8kHz, the sys.RtIntPeriod is 0, and the Coord[x].SegMoveTime is set to 1. We are running the same path every cycle however we are translating the path (X, Y and Theta) on a part to part basis. Quote Link to comment Share on other sites More sharing options...
steve.milici Posted January 26 Share Posted January 26 Your settings are relatively high frequencies and are probably not be the source of the “15ms” delay you see. I would suspect your “translation” as the culprit. This would be a technical support issue. Please contact ODT's direct technical support with your full issue details at: ODT-Support@Omron.com Quote Link to comment Share on other sites More sharing options...
Recommended Posts
Join the conversation
You can post now and register later. If you have an account, sign in now to post with your account.