RafaelFalcaro Posted March 2 Share Posted March 2 Hello, I'm using PowerPMAC's ISR interrupt to perform axes position acquisition, with the trigger source being the UserFlag signal. The implementation is functional, however the interrupt is being executed at each edge of the trigger, regardless of its direction (rising or falling). I would like the interrupt to happen only on the falling edge of the UserFlag signal. Here are the settings I made: Gate3[0].IntCtrl = $10000 Gate3[0].Chan[0].CaptCtrl = 10 Gate3[0].Chan[0].CaptFlagSel = 3 Gate3[0].Chan[0].CaptFlagChan = 0 UserAlgo.CaptCompIntr = 1 Here is the code inside the ISR: void CaptCompISR (void) { volatile GateArray3 *MyFirstGate3IC; // ASIC structure pointer int *CaptCounter; // Logs number of triggers int *CaptPosStore; // Storage pointer MyFirstGate3IC = GetGate3MemPtr(0); // Pointer to IC base CaptCounter = (int *)pushm + 65535; // Sys.Idata[65535] CaptPosStore = (int *)pushm + *CaptCounter + 65536; *CaptPosStore = MyFirstGate3IC->Chan[0].HomeCapt; // Store in array (*CaptCounter)++; // Increment counter MyFirstGate3IC->IntCtrl = 1; // Clear interrupt source } Quote Link to comment Share on other sites More sharing options...
Sangmo Posted March 5 Share Posted March 5 You can check the bit11 of Gate3[i].Chan[j].Status after entering the ISR function. If bit11 is 0, it means that the edge signal that triggers the interrupt is a falling edge. Quote Link to comment Share on other sites More sharing options...
RafaelFalcaro Posted March 6 Author Share Posted March 6 (edited) Hi @Sangmo, thanks for the reply! So I understand that the ISR function is executed on any edge of my trigger signal, is that right? I'm asking because in the Power PMAC User Manual (page 787) there is an information that for PMAC3-style ICs the detection is done via “edge-triggered” capture logic: If this is correct, what is the need to configure the Gate3[0].Chan[0].CaptCtrl register, since it only matters which trigger source (Gate3[0].Chan[0].CaptFlagSel)? Edited March 6 by RafaelFalcaro Quote Link to comment Share on other sites More sharing options...
steve.milici Posted March 8 Share Posted March 8 Logic based on the value bit11 in Gate3[i].Chan[j].Status would need to be added to the ISR. Quote Link to comment Share on other sites More sharing options...
rleoni Posted March 15 Share Posted March 15 Hello, I am working with Rafael on this issue and we solved the edge detection problem by setting Gate3[0].EncClockDiv. Quote Link to comment Share on other sites More sharing options...
steve.milici Posted Wednesday at 06:31 PM Share Posted Wednesday at 06:31 PM Good to know ... I should have suspected that!😬 Quote Link to comment Share on other sites More sharing options...
Recommended Posts
Join the conversation
You can post now and register later. If you have an account, sign in now to post with your account.