Hello, I am currently working on Clipper PLUS T3 controller.
It is an 8axis clipper .
I am using amp 1,2,3 as a milling machine.
I want to integrate the spindle to the PMAC Controller and require DAC output.
From the thread below I setup I variables.
Looked at this thread but could not find an answer
http://forums.deltatau.com/showthread.php?tid=185&highlight=spindle+clipper
Same as the thread I would like to use DAC output from axis 6.
This is what I set
I7100=1090
I7101=5
I7102=3
// Output Mode , PWM
I7126=0 ; default
// Maximum Output
I669=1090 ; DAC limit 10 Vdc
Then (I600=0 (motor not active)) M602=545
however it did not show 5V.
From the manual I found out that output6A(amp6 a output) is pin #4 but is it correct?
If I set I600=1 Other pins have Voltage according to the manual but pin 4, 5 is always zero.
Can anyone help with this issue?