I'm currently working on a project using a Delta Tau MACRO control system, but I've run into a bit of a roadblock:
Currently, the system includes a Delta Tau PMAC TURBO ULTRA-LITE Command card installed in a Windows Computer, an ACC-68M, and 2 ACC-85M cards, driving SGDV-R90AE1A and SGDV-2R8AE1A Servopacks. I don't have much real estate to work with for placing electrical components, so much so that I've had to resort to mounting parts transversally. I also require a significant number of Analog I/O pins for sensors and controls. Is there a product that is about the same size as an ACC-68M, is mounted and connected in a similar fashion, and can operate on the MACRO chain?