Jump to content
OMRON Forums

eloew61

Members
  • Posts

    4
  • Joined

  • Last visited

Everything posted by eloew61

  1. Forgive my ignorance, but will a "dwell" command work in this context?
  2. steve.milici, thanks for your advice. Motor[x].PowerOnMode is set to 0 for both motor 1 and motor2.
  3. We are using an ACC-14E interface to a PPMAC to provide absolute position for two axes via synchro to digital (S/D) converters. When the PPMAC is first powered on, PLC1 is executed which performs a homez on both motor axes using the following code: Motor[AZ_MOTOR_NUMBER].pAbsPos=ACC14E[0].DataReg[0].a Motor[EL_MOTOR_NUMBER].pAbsPos=ACC14E[0].DataReg[3].a Motor[AZ_MOTOR_NUMBER].AbsPosFormat=$00200F08; Motor[EL_MOTOR_NUMBER].AbsPosFormat=$00200F08; Motor[AZ_MOTOR_NUMBER].AbsPosSF=1.0; Motor[EL_MOTOR_NUMBER].AbsPosSF=1.0; Coord[1].PosRollOver[0]=360.0; Coord[1].PosRollOver[0]=360.0; homez AZ_MOTOR_NUMBER; homez EL_MOTOR_NUMBER; This routine correctly initializes the absolute position about 20% of the time. At other times, the position is exactly twice what it should be. When this occurs, acc14r0, acc14r1, acc14r3 and acc14r4 all contain the correct 16 bit angles; however #1p and #2p contain twice the angle, respectively. Re-running PLC1 from the IDE command line fixes the problem. I have attached before and after IDE screenshots of this.
  4. When performing a two-way step move using the tuning tool (Position Interactive), the load moves the desired number of counts in the positive direction, stops, and fails to return to the initial position. The move then times out without a plot. When performing a one-way step move, the load moves the desired number of counts in the positive direction, stops, then the move times out without a plot. Can anyone explain this behavior?
×
×
  • Create New...