cmcdonald
Members-
Posts
23 -
Joined
-
Last visited
Content Type
Profiles
Forums
Events
Downloads
Everything posted by cmcdonald
-
Where can I find a download for PeWin32 Pro? The Delta Tau web site now forwards to Omron website and I cant find anything with their search. THanks Chris
-
EtherCAT: ecatsdo write fails from terminal, works from etherlab
cmcdonald replied to andyf's topic in Power PMAC
Try disabling the ethercat. Then try the commands. Ecat[0].enable=0 I had the same thing. I had to use the ecatTypedSDO instead. Chris -
If I am not commutating can the UVW inputs (J7 MMACH3)be used for general purpose input? I'm using a Turbo Clipper. Thanks Chris
-
Does anybody have a good way to hand G20 and G21 inside the Prog1000 for Gcode implementation? I have a customer that had inch and metric g code files and refuses to convert them to one standard. Thanks Chris
-
Does anybody have a good way to hand G20 and G21 inside the Prog1000 for Gcode implementation? I have a customer that had inch and metric g code files and refuses to convert them to one standard. Thanks Chris
-
GetVectorVelocity() (current feedrate) in PLC
cmcdonald replied to RomanSolonto's topic in Turbo PMAC
I think M160 and M260 have to be multiplied by 3/(I108*32) to get into counts/mS Chris -
No, Mxx62 is my actual position. I need to compare the captured position from Mxx03 which rolls over sooner than Mxx62. I may have to come up with another approach to keep Mxx62 and Mxx01, Mxx03 in sync so i can do calculations. Is there a way to 'Zero' Mxx01? Chris
-
Actually M101 (ENC1 24-bit counter position) rolls over so when I use the captured position there is no way that I know of to reference the current position. Anybody know of any tricks? Chris M
-
I have an application that has a belt with a trigger that I capture the encoder position. This seems to work well until I have to preform a HOMEZ on the belt to ensure i don't rollover on the position counter. The problem is when i use HOMEZ the Encoder home capture position is not updated so i have NO reference from the Encoder Capture position to the actual position anymore. Does anybody have a solution? Thanks Chris
-
Yes it does. But it has to use a different port. The S7 requires another Modbus Server Rung. We are still having random Modbus disconnects (1-2 a day) and are in the process of using the PC software to check if the Modbus server is working on port 502 but we cant access 502 because the clipper is connected constantly. I would like to connect get data then disconnect from the server but Im not sure if that is possible. Chris
-
I have a clipper set up successfully as a Modbus Client to a Siemens S7-1200 (Server). Once I introduce another device (pc software)on the network it cannot connect unless i unplug the Ethernet connection to the Clipper. It seems that the clipper is holding the connection to the PLC. I have tried to increase the Timer in the MODBUS command setup but it seems to stay connected to the PLC all the time thus blocking any connections to the PLC. Is there a way to have the Clipper disconnect so that other devices can connect to the server? Thanks Chris
-
Is the Position window. I also see an RTI error in the Global Stats tab. What can cause and RTI error? Chris
-
We have a Motion Program that Homes a X Y Y' gantry. Our PC HMI initiates the homing program (It completes fine)then POLLS the P_HOMING_ROUTINE_COMPLETE bit (P50) to see if the homing is complete. IN PWIN We often get a Buffer is Open message while the machine is homing and we cannot poll for the P_HOMING_ROUTINE_COMPLETE bit. I can manually type CLOSE in the terminal and it will close the buffer. My question is what internally happens inside the controller when a HOME command is used? When I remove the last 'final' home command I do not have this buffer open [/php]issue. Thanks Chris McDonald #include OPEN PROG 101 CLEAR P_HOMING_ROUTINE_COMPLETE=0 P_MOTOR1_HOME_STATUS = 1 P_MOTOR2_HOME_STATUS = 1 P_MOTOR3_HOME_STATUS = 1 IF (ESTOP_Button=1) ; IF ESTOP IS ON DON'T HOME ;mathias #2 home plc I325=$78010 ; USE MOTOR 3 LIMITS TO HOME I126=16000 ;Motor 1 - Home Offset 1mm dwell10 IF (MLIM1_flag=1) ;motor 1 at home? dwell10 I123=50 ;reverse homing I7012=10 ;look for falling edge HOME1 ;reverse home dwell10 ENDIF IF (MLIM2_flag=1) ;MOTOR 2 already at home? dwell10 I223=50 ;reverse homing I7022=10 ;look for falling edge COMMAND"#3k" ;kill motor 3 to prevent lock up HOME2 ;reverse home dwell50 COMMAND"#3J/" ;renable motor 3 after home ENDIF I325=$78010 IF (MLIM3_flag=1) ;MOTOR 3already at home? dwell10 I323=50 ;reverse homing I7032=10 ;look for falling edge COMMAND"#2K" ;KILL MOTOR 2 TO PREVENT lockup HOME3 ;reverse home dwell50 COMMAND"#2J/" ;renable motor 2 after home ENDIF I120=200 ;Motor 1 HOME TA I121=50 ;Motor 1 HOME TS I123=-100 ;Motor 1 Homing Speed And Direction I7012=2 ;Servo IC 0 Channel 1 Capture Control I7013=2 ;Servo IC 0 Channel 1 Capture Select Control I126=-16000 ;Motor 1 - Home Offset 1mm ;I226=111072 ;Motro 2 - Home Offset 3501 um I226=-1000 ;(611+2000)*16 I220=200 ;Motor 2 HOME TA I221=50 ;Motor 2 HOME TS I223=-100 ;Motor 2 Homing Speed And Direction I7022=2 ;Servo IC 0 Channel 2 Capture Control I7023=2 ;Servo IC 0 Channel 2 Capture Select Control ;I326=109696 ;Motor 3 - Home Offset 6946 um I326=-16000 ; I320=200 ;Motor 3 HOME TA I321=50 ;Motor 3 HOME TS I323=-100 ;Motor 3 Homing Speed And Direction I7032=2 ;Servo IC 0 Channel 3 Capture Control I7033=2 ;Servo IC 0 Channel 3 Capture Select Control DWEll10 HOME1..3 dwell10 I120=200 ;Motor 1 HOME TA I121=50 ;Motor 1 HOME TS I123=10 ;Motor 1 Homing Speed And Direction I7012=10 ;Servo IC 0 Channel 1 Capture Control I7013=2 ;Servo IC 0 Channel 1 Capture Select Control I126=16000 ;Motor 1 - Home Offset 1mm ;I226=111072 ;Motro 2 - Home Offset 3501 um I226=16000 ;(611+2000)*16 I220=200 ;Motor 2 HOME TA I221=50 ;Motor 2 HOME TS I223=10 ;Motor 2 Homing Speed And Direction I7022=10 ;Servo IC 0 Channel 2 Capture Control I7023=2 ;Servo IC 0 Channel 2 Capture Select Control ;I326=109696 ;Motor 3 - Home Offset 6946 um I326=16848 ; I320=200 ;Motor 3 HOME TA I321=50 ;Motor 3 HOME TS I323=10 ;Motor 3 Homing Speed And Direction I7032=10 ;Servo IC 0 Channel 3 Capture Control I7033=2 ;Servo IC 0 Channel 3 Capture Select Control DWEll10 HOME1..3 P_MOTOR1_HOME_STATUS = 0 P_MOTOR2_HOME_STATUS = 0 P_MOTOR3_HOME_STATUS = 0 P_HOMING_ROUTINE_COMPLETE=1 ;SENDP"Homing X, Y End" I124=$8001 ;enable limits for motor1 AND ENABLE AMP FAULT I224=$8001 ;enable limits for motor2 AND ENABLE AMP FAULT I324=$8001 ;enable limits for motor3 AND ENABLE AMP FAULT ;I325=$78008 ; USE MOTOR 2 LIMITS I114=-1 ;Motor 1 - Software Position Limit I214=-1 ;Motor 2 - Software Position Limit I314=-1 ;Motor 3 - Software Position Limit I113=1229566 ;set pos limt 48.4" I213=945657 ;set pos limt I313=945657 ;set pos limt ELSE P_HOMING_ROUTINE_COMPLETE=0 ; FAIL Homing ENDIF CLOSE
-
Is there a way to to create a deployment package just to install PCOM server and its support files and PWIN only? We are trying to create an installation disk for our software (we do have the development package) but I don't want our customers have to install the full suite. Thanks Chris
-
Is there a way to get a axis definition into a P or M variable? I want to a plc to calculate a scale factor based on the axis definition. I have several machines that i want to update and they have different axis definitions (gear ratios) for motor 1 and motor 2. Thanks Chris M
-
I read that PMAC-NC Designer is only compatible with window XP. Has anybody gotten the NC software to run on an Windows 7 32 bit machine? Thx Chris
-
Since we have tight tolerances to hold to, its best we don't change the trajectory of the path at all. With my experimentation the TA/TS value to get the fastest cycle time with lowest following error shows that A low TA/TS (20/10) and A feedrate of 500 mm/s works well with laser cutting a 1mmx1mm square but if I run a 100mmx100mm square at the same TA/TS and feedrate i get alot of 'jerk' or knocking in the corners and my following error goes up. SO I need to rincrease the TA/TS of the larger squares to get the fastest cycle time. I need a way to do this automatically or is there a feature in the controller to help this? Is there a way to factor in the length of travel in to this formula TA=2*Radius/Feedrate? It seems i would get the same results for a 1mm square or a 100mm square. I've also experimented with turning the blending on and use the following settings so that we blend certain LINEAR moves that are over a certain angle. Does this work well enough? Isx82 Coordinate System ‘x’ Blend Disable Dwell Time Isx83 Coordinate System ‘x’ Corner Blend Break Point Isx85 Coordinate System ‘x’ Corner Dwell Break Point Thanks Chris
-
We are doing this manually and it works. I was wondering if there was some formulas out there to calculate how much to increase TA/TS. Some of our customers have 1000's of different shapes and sizes so we want this done automatically. Thanks Chris
-
I am already using the look ahead feature. I'm using I5113=5 and I5120=50. And because it is important to hold the cutting path we are using DWELL0 on most of the LINEAR moves. Chris
-
I am working on a high speed laser cutting application using linear motors. We are controlling X X' & Y gantry and we are using the Linear and circle commands. With this application we have a lot of small moves mixed in with larger moves. These small moves need a Low TA TS for the smaller moves to complete quicker. When we use a the same TA TS for the larger moves we get a lot of jerk in the system. I was wondering if anybody has some experience the dynamically changing the TA/TS to eliminate Jerk based the type of move. The goal is to optimize the cycle time with the least jerk and following error. Thanks Chris
-
Hi, I'm working with the binary rotary buffer using the [i]DPRAsciiStrToRotEx[/i] function (i.e. [i]DPRAsciiStrToRotEx(dwDevice,str,coordSys,sendImmediate,status)[/i]), but it doesn't seem to work and I'm getting a [i]-70[/i] for the "status", for which I can't find the specific reference in the documentation. In the documentation, it seemingly suggests that it is a conversion issue, but the same program lines have worked fine previously. I'd like to know what error that status value implies and how to fix it. Thanks, Chris
-
I have an application that controls the position of a sheet of glass with 2 conveyors. Motor 2 and Motor 3 and their encoders are hooked up as normal. I have the motors in the same coordinate system (Y) . No I want a master encoder (wired to the HandWheel A+/A- B+/B-) that will roll on top of the glass to have final control over the position of the glass in case of slippage on the conveyor. How do I set up my 2 motors to use this master encoder? I'm rather new to the Turbo Pmac (using a clipper). Thanks Chris