MartinOphey
-
Posts
12 -
Joined
-
Last visited
Content Type
Profiles
Forums
Events
Downloads
Posts posted by MartinOphey
-
-
Thanks
-
If i lost the configured ip adress how i can reset it over rs232, which tool is needed?
-
what is the function behind this two files?
-
-
Perfect, thanks!
-
How I can save variables remanently?
-
Is it possible to watch the commanded position before it is filtered by pre-notch-filter?
I have programmed a spline move with motion programm to create a asymmetric sine wave. The motion programm spline between sine reference points.
If I use the pre-notch-filter the original reference position is not the same like commanded position of motor.
I do not want to create a phantom motor for this.
-
Am I right, that it is necessary to make a power off/on to reset the c written rti code? Also the C-Variables.
I have got a feeling that the "$$$***" resets only the the Power PMAC Script Language written code.
-
Ok, that means there is no way to look c-variable directly?!
Because the discribed way takes a lot of time if my code is big and i have a lot of variables.
-
How I can watch lokal C-Variables form rticplc.c?
Regarding the folowing sample: stiffness1
#include #include #include #include #include #include "../../Include/pp_proj.h"const double pi = 3.1415926535;void simulation(void);void realtimeinterrupt_plcc(){simulation(); }void simulation(void){//input variables for simulation double mass, freq1; //output variablesint feedback1;//simulation constantsdouble stiffness1; .... //copy parameters from P-variables to double variables mass = GetGlobalVar (pSimMass); ... stiffness1 = 2 * pi * pi * freq1 * freq1 * mass; feedback1=.... .... //set the simulation output parameters: feedback positions SetPtrVar (mSimMotor1FeedbackPos, feedback1);}
Thanks
-
I need the actual Power PMAC Server. Where i can find it?
lost configured ip adress
in Power PMAC
Posted