Hi,
encoder line should be encoder line spacing, which, in your case, should be 50nm.
electircal cycle (or commutation cycle) means the distance between your poles.
Phase position resolution is the smallest unit of your hardware count.
Example :
A linear brushless motor has a commutation cycle of 60.96 mm (2.4 inches). It has a linear scale with a
20-micron line pitch. The scale is used for both commutation and servo feedback.
The commutation uses the hardware counter. There are 200 hardware counts per millimeter (5 microns
per count), so 12,192 hardware counts per commutation cycle. Ix70 should be set to 1, and Ix71 should
be set to 12,192.