I have a clipper drive unit and I am seeing strange peaks in the CPU resources graph. The phase frequency load (red bar) regularly jumps to up to four times the continous load.
The peak values are depending on the frequency settings as described below. It peak seems to be related to the PWM frequency. The unit is running just by itself by 24PSU, no cables or busvoltage attached.
If I do these tests with the same parameters on a Geobrick-LV with identical firmware version (but without Macro IC0) or with a stand-alone Clipper (just 5V PSU), I do not see this phenomenon, there are no clear peak loads observed. Unfortunatly, I cannot simply swap the Clipper boards.
I100,4,100=1 ; I101,4,100=1
a) PWM=36kHz, phase=36kHz, servo=4.5kHz (I7000=817, I7001=1, I7002=7).
Continuous phase load = 32%, peak load = 132%
b) PWM=36kHz, phase=18kHz, servo=4.5kHz (I7000=817, I7001=3, I7002=3).
Continuous phase load = 18%, peak load = 132%
b) PWM=18kHz, phase=36kHz, servo=4.5kHz (I7000=1634, I7001=0, I7002=7).
Continuous phase load = 32%, peak load = 66%
Measurements are done without motors enabled.