Do you do a build and download or only a build? At the end of a build or a build and download we print in the output window all the messages that are generated by the build and download and also we print the total time for build and also the total time for the download process as well, can you share those numbers. I want to see whether the build is taking the time or the download. For the build process portion of the build and download, we upload the libraries from the Power Pmac one time during your first build or build and download process. After the initial upload, the subsequent builds only check the type of the PMAC you are connected to generate the correct make files for the build, which would not consume any time at all.