Jump to content
OMRON Forums

Hersoft

Members
  • Posts

    7
  • Joined

  • Last visited

Everything posted by Hersoft

  1. Hello, I have an ACC-5E which has a missing component on the back of the card. the missing component is U23. could someone who has the same card make a picture of the component for me or give me an exact description of the smd-code on the part? That would really help me out. Much regards, Otto Hering
  2. Hersoft

    ACC-5E

    Hello Sina, Here are the serial numbers. ACC-5E (603447-101) S/N: C0007EQD 3U-Turbo (603766-104) S/N:C0003VNZ V1.942 5C0 (option) I tried the ACC-5E also with a different CPU but this did not change the situation. I hope this helps somewhat. Regards, Otto.
  3. Hersoft

    ACC-5E

    Hello Sina, well I did just that and checked the value of I4902. It came back wit $0 which can not be true i guess. I put the card on the first address of the table and I got the Macro chip on it. Any suggestions now? regards, Otto.
  4. Hersoft

    ACC-5E

    Hi there, I just got an ACC-5E and want to use it for a couple of things. Mainly for the handwheel input and for the Display output. When I put the board into my UMAC chassis and start UMAC configuration software I had expected to see an extra (unidentified maybe) I/O board or an Macro board. I made sure there where no other boards in the chassis except for the Turbo Pmac and ofcourse the PSU. Because I do not see any extra boards I think my ACC-5E is broken. Is there any way to check it further? Regards from Belgium, Otto.
  5. Hello Steve, oke, the spindle setup is now working. From the software operator panel it is now possible to switch on/off the spindle and to select the direction. also from the m-codes this is now working correctly. for the hanwheel i still need to do some hardware work so this will take me a bit longer. thanks for your help, regards.
  6. [quote='steve.milici' pid='1128' dateline='1295460794'] This is already in the spindle PLC created by the NC-Setup program when you selected the software control panel. It should have a red 'Spindle On' button. Yes you can use this channel for your hanwheel. The HANDLE_COUNT_M variable in the HANDLE.PLC needs to point to your processed handwheel counter. [/quote] Hello Steve, thanks for your speedy reply. Hmm, I think my problem lies in the fact that I want to use ACC-11E output 1 to control my spindle on/off and I use M7024 for this. When I browsed through the Address.h file i saw that the spindle is normally controlled via M65 (open loop) and M85(closed loop). should I include the io810.h file for my definitions for the ACC-11E ? I need to do some work before the handwheel caqn be connected so I can not test this right now. When possible I will get back to the forum about this. Regards, Otto Hering.
  7. Hello, I'm fairly new to Delta tau so forgive me if my questions seems stupid. I'm in the process of converting my mill from a PMAC-PC (ISA) to the UMAC based Turbo PMAC. my config in the UMAC -box is as follows: -ACC-54-USB -PMAC Turbo -ACC-24E2A four ports -ACC-11E I/O -ACC-36E analog inputs (spare for now) -ACC-E1 this all in a 16 slot enclosure. I have another ACC24E2A four-port version and an ACC24E2A two port version on spare. - WSDI BPU-S5 for X, Y and spare - WSDI BLU-S1 for Z and spare. -Bell-Everman Lowboy 1060 on the X-Axis -Bell-Everman Lowboy 760 on the Y-Axis -NEAT/Parker slide with Servo on the Z-Axis Tuning was no problem, loop is tight and stable. Limit switches are working and installed, home switches are working but have to be installed yet (soon) I/O, I am able to manually switch-on/off ports on the ACC-11E via M-codes in the terminal window of PMAC-NC. I/O, I am able to detect input signals on the ACC-11E also. I have already succesfully setup the system for use with the latest version of PMAC-NC Pro2 I am running PMAC-NC Pro2 on a computer with the software control only. I am able to run g-code progs and the machine is executing them in a correct way. Axis set-up is correct. My questions are: - How do I implement the manual control of the spindle on/off (M7024) for the software control panel? I did try to insert it into the cntlpanel.plc but that did not work. - I would like to connect an manual pulse generator (handwheel) with A and B outputs. I understand from the forum that I could use my fourth ACC-24E2A Encoder input for this. Nice! but how? I probably also need to set-up an PLC for this, again how? as you probably have guessed I'm not a professional user but I have learned by doing (and making mistakes) and have come a long way since my first start with the PMAC-PC. Converting to the UMAC system was a big thing and I'm almost there now, just these extra little things to make it perfect. any comments would be higly appreciated! Regards, Otto.
×
×
  • Create New...