Hersoft
-
Posts
9 -
Joined
-
Last visited
-
Days Won
1
Content Type
Profiles
Forums
Events
Downloads
Posts posted by Hersoft
-
-
Hello Steve,
On the Barcode sticker placed on the Slot connector it states: C0007EQD
is this sufficient or should I take a picture?
regards, Otto Heering
-
Hello,
I have an ACC-5E which has a missing component on the back of the card.
the missing component is U23.
could someone who has the same card make a picture of the component for me or
give me an exact description of the smd-code on the part?
That would really help me out.
Much regards, Otto Hering
-
ACC-5E
in Turbo PMAC
Hello Sina,
Here are the serial numbers.
ACC-5E (603447-101) S/N: C0007EQD
3U-Turbo (603766-104) S/N:C0003VNZ V1.942 5C0 (option)
I tried the ACC-5E also with a different CPU but this did not change the situation.
I hope this helps somewhat.
Regards, Otto.
-
ACC-5E
in Turbo PMAC
Hello Sina,
well I did just that and checked the value of I4902.
It came back wit $0 which can not be true i guess.
I put the card on the first address of the table and I got the Macro chip on it.
Any suggestions now?
regards, Otto.
-
ACC-5E
in Turbo PMAC
Hi there,
I just got an ACC-5E and want to use it for a couple of things.
Mainly for the handwheel input and for the Display output.
When I put the board into my UMAC chassis and start UMAC configuration software I had expected to see an extra (unidentified maybe) I/O board or an Macro board.
I made sure there where no other boards in the chassis except for the Turbo Pmac and ofcourse the PSU.
Because I do not see any extra boards I think my ACC-5E is broken.
Is there any way to check it further?
Regards from Belgium, Otto.
-
Hello Steve, oke, the spindle setup is now working. From the software operator panel it is now possible to switch on/off the spindle and to select the direction. also from the m-codes this is now working correctly. for the hanwheel i still need to do some hardware work so this will take me a bit longer. thanks for your help, regards.
-
[quote='steve.milici' pid='1128' dateline='1295460794'] This is already in the spindle PLC created by the NC-Setup program when you selected the software control panel. It should have a red 'Spindle On' button. Yes you can use this channel for your hanwheel. The HANDLE_COUNT_M variable in the HANDLE.PLC needs to point to your processed handwheel counter. [/quote] Hello Steve, thanks for your speedy reply. Hmm, I think my problem lies in the fact that I want to use ACC-11E output 1 to control my spindle on/off and I use M7024 for this. When I browsed through the Address.h file i saw that the spindle is normally controlled via M65 (open loop) and M85(closed loop). should I include the io810.h file for my definitions for the ACC-11E ? I need to do some work before the handwheel caqn be connected so I can not test this right now. When possible I will get back to the forum about this. Regards, Otto Hering.
-
Hello, I'm fairly new to Delta tau so forgive me if my questions seems stupid. I'm in the process of converting my mill from a PMAC-PC (ISA) to the UMAC based Turbo PMAC. my config in the UMAC -box is as follows: -ACC-54-USB -PMAC Turbo -ACC-24E2A four ports -ACC-11E I/O -ACC-36E analog inputs (spare for now) -ACC-E1 this all in a 16 slot enclosure. I have another ACC24E2A four-port version and an ACC24E2A two port version on spare. - WSDI BPU-S5 for X, Y and spare - WSDI BLU-S1 for Z and spare. -Bell-Everman Lowboy 1060 on the X-Axis -Bell-Everman Lowboy 760 on the Y-Axis -NEAT/Parker slide with Servo on the Z-Axis Tuning was no problem, loop is tight and stable. Limit switches are working and installed, home switches are working but have to be installed yet (soon) I/O, I am able to manually switch-on/off ports on the ACC-11E via M-codes in the terminal window of PMAC-NC. I/O, I am able to detect input signals on the ACC-11E also. I have already succesfully setup the system for use with the latest version of PMAC-NC Pro2 I am running PMAC-NC Pro2 on a computer with the software control only. I am able to run g-code progs and the machine is executing them in a correct way. Axis set-up is correct. My questions are: - How do I implement the manual control of the spindle on/off (M7024) for the software control panel? I did try to insert it into the cntlpanel.plc but that did not work. - I would like to connect an manual pulse generator (handwheel) with A and B outputs. I understand from the forum that I could use my fourth ACC-24E2A Encoder input for this. Nice! but how? I probably also need to set-up an PLC for this, again how? as you probably have guessed I'm not a professional user but I have learned by doing (and making mistakes) and have come a long way since my first start with the PMAC-PC. Converting to the UMAC system was a big thing and I'm almost there now, just these extra little things to make it perfect. any comments would be higly appreciated! Regards, Otto.
ACC-5E component identification
in Turbo PMAC
Posted
Steve,
Thank you very much, you are my hero.
I'll know now what to put ther on that location.
Regards, Otto Hering.