paison
-
Posts
38 -
Joined
-
Last visited
Content Type
Profiles
Forums
Events
Downloads
Posts posted by paison
-
-
hello:
I want to know how to protect the integrity of the controller powerpmacproject. Turbo PMAC can set the password. The problem is that power has set the password, but there is no way to restrict the anonymous access of the user powerpmacproject
User powerpmacproject can be deleted and modified at will through anonymous access, which I think is unsafe.
-
I want to know how to protect the integrity of the controller project. Turbo PMAC can set the password. The problem is that power has set the password, but there is no way to restrict the anonymous access of the user project.
-
I found a problem that powerpmac does not need any privileges to access files in userflash directory. It does not need a password to access files. There are project files in this directory that can be deleted and modified arbitrarily.
-
I have the same problem with you. I tried to download my project with the compiler and download routine in PDK, and found that it was not as stable and reliable as IDE.
-
Thanks Steve
-
hello :
I want to know what instructions "list gather" in Turbo PAMC use in powerpmac instead.
-
thanks your answer!!!
Sorry, maybe my description is a bit of a problem, my application is through the sensor in the object surface changes in three directions to determine the next moving target, similar to an unknown search movement, which need to move in the non-stop change the target location
-
hello everyone:
I would like to use pmac to develop three motion axes according to a sensor to determine the next movement of the target position, which requires an initial target, according to the sensor dynamic changes adjust the movement of the target, how to achieve this? Who has a good idea to share with me, thanks!
-
Thanks for your answer,When HMZ is called, if the call triggers the latch, how does the latch change into the encoder location?
-
hello everyone:
If the No. 1 axis calls # 1hmz, how will the encoder position and motor position be converted?
-
hello everyone:
I want to get one can achieve by setting the interval of the output of a series of pulses in the process of two-dimensional curve movement, used to trigger the laser measurement, I think the comparison function of PMAC can do it, but the information I still don't understand his specific usage, who can give me a specific example of Cliper PMAC, thank you very much
-
hello:
Who can provide me with a Pcommserverpro2 manual, or Pcommserverpro2 manual download address, I can not find his official website of the download, thank you
-
Thank you for your reply, the second solution should be more perfect
-
hello :
I have a problem with a zero offset if the IXX26 is set to a value greater than 8388608, what good solution?
-
i think Q variable and P variable function is different, even if there is only one coordinate system, q variable and coordinate system closely related
-
Thank you for your reply, I see in the PWINPRO32 variable watch window, my system only specifies a coordinate system.
-
Hello:
When pmac has only one coordinate system, what is the difference between p variables and Q variables in use? I found that Q variables often switch between 0 and the specified value, I would like to know what is the cause, how should I avoid this problem, Q variables can be used in PLCC0?
-
I would like to ask, if it is Clipper + ACC1p optional1, ACC1p IO and pc104 the IO address the same?
-
hi:
i want to know ACCIP IO addresses and how to define them?
-
hi:
If I use the HMZ to clear the latch position and the actual position is very different, what should I do to make the latch position correct?
for example:
m162 = 125000
m103 = 22250
How to correct the conversion?
-
Thanks !!!
-
hi:
Remove Lookahead, if you want to open Lookahead again, how should be how to operate in order to enable the Lookahead function normally open?
-
Thanks,I have sent a message to deltatau
-
Reading Motion Prog
in Power PMAC
Posted