sutty
-
Posts
80 -
Joined
-
Last visited
-
Days Won
2
Content Type
Profiles
Forums
Events
Downloads
Posts posted by sutty
-
-
Hi Unit101 and others!
Curt Wilson has sent me an answer:
There are two reasons for the difference.
First, the Motion Machine uses an i7 processor, which is much faster than the ARM embedded processor used in the CK3E. (It is also much more expensive and much more power hungry.)
Second, the Motion Machine uses the stripped down Etherlabs EtherCAT stack software, which is very efficient at the cyclic communications, but lacks many of the features – both in setup and execution – of the Acontis stack used in the CK3E.
Thanks for sharing this excellent real world data !
I will watch for experts reply... I suspect the difference is that the MM has a more powerful cpu....
-
-
Hi there!
I am testing one and the same Application (w EtherCAT: 22 axis, IOs) on 2 different Power PMAC HW:
1. Motion Machine
Motion Core LX86
1097.554 MHz
dual core
Kernel Version 3.14.28-xenomai-2.6.4
FW 2.1.0.27
Total mem 3922 MB
Free mem 3260 MB
2. CK3E
uPower PMAC
arm.LS1021A
1000 MHz
dual core
Kernel Version 3.14.28-ipipe
FW 2.2.0.37
Total mem 1007MB
Free mem 556 MB
Benchmarking (CPU-usage):
Motion Machine: FG 10.7%, BG 21.8% Yield to OS 167.6%
CK3E: FG 38.7%, BG 71.4% Yield to OS 89.9%
How come there is such big difference between both CPU-types?
Is there any official benchmarking for Delta Taus different Power PMAC types?
Regards, Anton
-
Hi!
I am cascading 2 motors using motor #1 for the outer loop (position), #21 for the inner loop (velocity,current - direct PWM).
If cascading using method "Joining the Loops through Position Following Function" it all works fine. But using method "Joining loops directly" (exactly after Users Manual p. 338) the net desired position of motor #21 is not overtaking its ActiveMasterPos-value at all (see http://forums.deltatau.com/showthread.php?tid=2087&highlight=activemasterpos)
System: UMAC Power PMAC ARM 2 Core (LS1021A) CPU Board ASSY 604112-10
FW: 2.2.0.37
Any idea?
Is there somebody with good results cascading 2 motors joining loops directly?!
Best Regards,
Anton
Benchmarking Motion Machine and CK3E with EtherCAT
in Power PMAC
Posted
Hi mbalentine!
Henry Bausley from ODT has sent me some more infos you also might be interested into:
"You can see from the numbers... [in the table below] even though the i7 is a better performer the CK3E does very well with the etherlab stack it was originally designed for.
The CK3E is not available for sale with the etherlab stack. The UMAC version of the ARM will have the etherlab stack present."