Good morning,
Trying to setup a Power UMAC to work with a drive in analog torque mode. In the System Setup tool when entering Amplifier Information, we choose Position Control = False, Velocity Control = False, and Torque Control = True. This opens up another section for Power Ratings.
Regardless of what values we enter, we get the error "Invalid max bus voltage, can not be 0 or empty! Cannot Update." This is step one in the motor setup tool, so without moving past this we can't continue with the setup.
The output tab says only:
system ethercat -m0 xml //1/28/2016 :9:38 AM - 192.168.0.200
system ethercat master // 1/28/2016 :9:38 AM - 192.168.0.200
Sys.MaxEcats = 1 // 1/28/2016 :9:38 AM - 192.168.0.200
See attached picture. We've tried every value we can think of and still get the same error.
Any advice on how we can move along here? Thanks!