Jump to content
OMRON Forums

Ariane

Members
  • Posts

    1
  • Joined

  • Last visited

Everything posted by Ariane

  1. Hello, I'm trying to develop a Python application that will control the Turbo PMAC2 and some other devices. This Turbo PMAC2 is installed inside a machine, and works very well with PWin32Pro2. I'm trying to use a dll to do this, is this the best option? I downloaded a lot of Turbo PMAC2 manuals, and I found the PComm32PRO manual: http://www.deltatau.com/manuals/pdfs/PCOMM32%20PRO.pdf?id=635415374139453187 But a think it's obsolet, it talks about the PComm32.dll, and some examples that should be in the library, but it doesn't exist. I found just the PComm32W.dll and PcommServer.exe (that starts when I try to open a communication with PMAC2). These two, PWin32PRO2, are installed by PMAC Executive Pro2 Suite. Sometimes my application works, and I can read and change the value of a P variable(it was all that I could do until now), but it's totally unstable. It just works when it wants. Is there a new manual or a example about how to do this? Is a dll the best option? *I can not uninstall PWin32PRO2. The machine must work in the both options without reconfiguration. **The conection is USB. Thank you!
×
×
  • Create New...