Jump to content
OMRON Forums

Bryan2112

Members
  • Posts

    2
  • Joined

  • Last visited

Bryan2112's Achievements

Newbie

Newbie (1/14)

  • First Post
  • Conversation Starter
  • Week One Done
  • One Month Later
  • One Year In

Recent Badges

0

Reputation

  1. Hi folks, I'm stuck with an old machine application that can't be installed on a higher OS than WinXP32 due to an issue with the security dongle. I'm running the application inside a VM on Win10. The problem is that when I try to install the IDE on XP, the installation halts saying that Internet Explorer 10 or higher is required, WinXP can only go to version 8. Is there a way around this problem? Thanks for any help you can offer. Bryan
  2. Hi folks, I've recently added some new equipment to a Z-Axis as part of an upgrade. This has added a fair bit of weight to the axis and the motor isn't coping too well as a result. There is another machine on site ( a Fanuc), that uses air assist which works really well, so, i'd like to try the same approach on the affected machine. Controller is a Turbo Pmac2 in a UMAC configuration. I've configured a spare output (M7135) and tested it ok. Could someone provide me with a code example on how to fire this output? Output to energise an air solenoid. Basically what is required is, once a counter-clockwise movement of the motor is detected, M7135 needs to go high. Motor is #3 in the system. Many thanks. Bryan
×
×
  • Create New...