windell747
Members-
Posts
119 -
Joined
-
Last visited
Content Type
Profiles
Forums
Events
Downloads
Everything posted by windell747
-
I just attempted to update my Power PMAC to the latest version XXX. After downloading and building my project, I attempted to upload my previous configuration (file attached), but I get an error. I had top save as a text file because the forum wouldnt let me attach. I've pasted the output below. /var/ftp/usrflash/Project/Configuration/042916_simulator_config.cfg:7:18: error #75: Struct Write Error: Sys.CPUTimerIntr=$1 Downloading Configuration Files Failed! Any idea what could be happening? 042916_simulator.txt
-
New release 2.1.0.107 crashes while motor tuning
windell747 replied to kandauru's topic in Power PMAC
I am having the same issue where the IDE (2.1.0.107) crashes when I attempt to do a open step response. Primary option: I know that i can do an update to my firmware to fix this, however right now I'm stuck at 1.5.8 since when I upgrade any higher, my code doesn't run correctly at it did before. So I always had to revert back Backup option: I believe that I was able to do the tuning fine with my old IDE (version 1.6.0.109) however, when I go to download filedepot to download it, the file is only about 9 mb in size. Where is it supposed to be ~700 mb in size. Is there a way I can get access to this old version of the IDE? thanks, windell -
Hi, What is the minimum system requirements for the IDE? Is there a list of firmware versions that are compatible with each IDE version? thanks, windell
-
Thanks for asking bgoskouie. Weʻll I did have the IDE running and I was using the watch window, but all I was looking at was two structure elements: Coord[0].ProgActive and Coord[1].ProgActive so there wasnʻt an abort anywhere in the watch window or a mistyped command.
-
Aloha, Iʻm attempting to use the sine sweep to determine my plant transfer function. Iʻve done a search on the forum and see references to the PMAC Servo Analyzer, but that was 5 years ago. So Iʻm wondering if the IDE can produce the Bode magnitude and phase plots from a sine sweep test? I understand that I can do individual sine tests, let the plant come to steady state and then manually and estimate the magnitude and phase, but Iʻm trying to see if there is a way to do this automatically. Thanks, windell
-
Aloha, Attached is a copy of the motion program that Iʻm running. I have a C program that starts it and pretty much never does an abort to stop it. However, Iʻve realize that after a few cycles of running it will stop itself. Iʻve verified that no following error or travel limit has occured. Iʻm wondering what could be going on here? How can I prevent it from stopping? The P_PVT_HA_TRACKING flag is toggled to a 1 or 0 by the C program and is dependent on how far away the axis is from the target. My thinking is that the linear move ends and doesnʻt see another move in front of it ready to execute and so the motion program ends. My firmware is 1.5.8 (I know its old, but upgrading has caused some problems that I donʻt have time to deal with at the moment. My goal is to upgrade soon) thanks, windell prog3.pmc
-
I certainly understand what you're saying about the JogTa limit because that is the way I interpret the setting when I read the SRM. Background: However, I have empirical evidence where 1 on 500 or so jogs will have a DesPos trajectory that violates its own acceleration limit by 2 to 3 times. Of course, I understand that it is not intended to do this, but I've tried all of your suggestions about things to check and monitor and the problem still remains. What seems to be a trivial thing is seems to not be so simple. Here are three threads in the past that I've raised about the issue. Initially, I had a race condition where large steps were making it into my pvt commands, but now I am certain that there is no race condition and the motion program is aborted before the jogs are called. http://forums.deltatau.com/showthread.php?tid=1972 http://forums.deltatau.com/showthread.php?tid=1987 http://forums.deltatau.com/showthread.php?tid=1884 What I've done: What I've gathered through conversations with Steve is that when a Jog is called it uses measured velocity, acceleration, and jerk values as the initial point for the Jog and propagates that forward. So encoder noise could create an issue so that the jog will plot a trajectory from a false velocity that was calculated due to noise. However when I speak with Curt, he says that encoder noise isn't an issue for the Jog trajectory since it is based on the last DesPos value right before the jog is called. So I'm a bit confused about the conflicting information. It seems that I'm missing part of the puzzle. What I'm doing now: From my previous conversations with you, you were saying that jogs aren't meant to blend with pvt commands. I understand this so I'm currently following your old suggestion to use linear mode and not stopping the motion program. I'm rewriting some of our code now to use linear mode as opposed to jog calls. So that is the status. Example: To provide you with a clear example of what I mean, I've attached a screen shot of a fault that we received on the night of 4/7. You will want to look at the red trace for the hour angle axis (the second plot). The red trace is the value of Motor[0].DesPos with time. The Y-axis is in degrees. X-axis is in seconds (Linux time). You'll also see that in the 5th plot, the current for the hour angle axis also saturates to 20A for this brief time. This current maxing out is the first sign that the trajectory is not right. When you go through the numbers, you get (2*(4.149638-4.12615 deg)*3600 arc-sec/deg)/(.123201 sec) = 1372 arc-sec/s^2. At 1035 motor units/arc-sec, I convert to milliseconds/motor unit we get a value of 0.7 ms^2/count. The value we have set for JogTa for this move is -2.41 ms^s/count. I'd be happy to speak with you on the phone to work directly with you on this issue. thanks, windell
-
Hi Charles, Thank you for your help. One of the road blocks is debugging the issue with the jog call that generates a trajectory that violates its own JogTa setting. The trajectory remains parabolic (Ts=0 for us) but just simply is too quick and generates a following error. 1) We currently have a separate background program that runs all night and logs Motor[x].DesPos (as well as a lot of other data) at 50 ms intervals, but the issue is that it has been difficult to effectively work with deltatau to resolve the issue because we don't use the high resolution Gather function. Instead we use the data logging by our separate process and currently have an offline program that we use to parse it manually when there is a problem to troubleshoot. If I can get a list of items of what DT would need to more effectively debug my situation so that I can provide the necessary data at the sample rate that you would desired then that would really help me. For faster sampling than 20 Hz maybe up to 100 Hz, I likely will need to create yet another separate process that samples for only a small window and has some smarts since continually recording data at a rate faster than 20 Hz might be storage repohibitive if doing so for the entire night. 2) Can you point me to where the application note that you are referring to is located? thanks, windell
-
Aloha, I have a trajectory generation issue with the jog that over accelerates the telescope and only occurs once every thousand or so jog calls. It is not predictable when it will occur. However, I want to do data gathers before each jog is called for X amount of servo cycles and stop. Unfortunately, since I don't know when the fault will occur, I will need to come up with a way to either store consecutive data gathers for the entire night (~500 jogs calls) or gather for the maximum amount of servo cycles and like a fault doesn't occur during that time, I overwrite the gather buffer. If it does occur during the set amount of time, then I store that data gather somewhere. I've read up on the Data Gather section in the Power PMAC Users Manual and looked at the training slides and it doesn't seem to go this advance. I'm wondering if anyone has an example of how to do this? thanks, windell
-
Motor[x].ActVel dropping to zero occasionally
windell747 replied to windell747's topic in Power PMAC
Looks like we're onto something. I will do that plot to see what is up. We have a max delta filter running in the encoder table for each of our encoders. Since the ActVel is for the motor position, I'm assuming that seeing these drops means that they are making it past this filter? thanks, windell -
Aloha, While moving our telescope I was watching the Motor[x].ActVel register in the IDE scope and saw that it was tracking the telescope velocity then it starts to briefly drop to 0 and then goes back up to the constant velocity that the telescope is at. What could be the causes of this? Is this register calculated from the Pos2 encoder entry? Could it be an encoder noise issue or corruption in bits from the absolute encoder? On the large scale it looks like the currents are fine so I'm not sure if the servo loop is being affect by this. thanks, windell
-
1) We do have the different encoder scaling factors such that the scaling is the same as seen by the motor. For the absolute encoder we keep the value at 1, and for the incremental we pretty much set the scale factor to counts_absolute/counts_incremental. So with no slip, they should read the same value. 2) Haven't tried putting the different encoders for the inner and outer loops. That does look like an attractive option. I'm troubleshooting an existing operational system so changing the way we use our encoders in the inner and outer loops might be somewhat of an uphill battle for me. I would need to be sure that this issue is caused by the encoder switching in order to get permission to modify how were using the encoders in the feedback loop. 3) This sounds like a position estimation scheme by using the virtual motor. It does sound interesting and I can see its benefits, but we haven't done anything to this exotic level. 4) In between two jogs what would the velocity, acceleration, and jerk be? Would the last trajectory velocity, acceleration, and jerk values be passed to be the initial conditions for the next consecutive jog?
-
Thanks Curt for explaining so clearly. 1) Here is my scenario. If a motor is currently running on a jog that is close to completing as it is getting close to the new position so its decellerating, then a) the encoders are switched to a different one, b) the servo gains are changed while acting on that encoder c) the HomePos is changed for that motor d) a jog command to a position is issued to a new position Would any of the stuff before the jog cause the derivatives to be miscalculated for the second jog? It would seem that from your previous response that the answer is no, but I just wanted to make sure that I was understanding right. 2) The reason I'm asking is that for our telescope application, sometimes (once in >1000) jogs, a jog is issued behind another jog and the acceleration of its trajectory is way faster than what is specified for the Jog.Ta and Jog.Ts values. It causes too much current to be drawn and we abort the motion. I want to note that the previous jog hasn't yet finished, so were pretty much updating the end point for the move by reissuing the jog. What is happening between the two jog calls is that we switch encoders, change the servo gains, and modify the HomePos for that motor. a) We switch encoders because we want the finer resolution when we get close to our target, but for big movements, we stay with a courser resolution. b) We change gains when we're close because we want a tight loop for velocity, but when were moving to a new target we ease off on the gains since the following error isn't critical. c) We modify the HomePos because the previous incremental encoder builds up error as it is mounted to the telescope via friction drive, so we do an absolute encoder (can't slip) read and adjust HomePos for the motor so that the motor position is now consistent with the absolute encoder read. Pretty much we zero out any incremental encoder error this way. 3) Say the motor is at a stop, but in closed loop and then a jog is called to move that motor to a new location. How does it calculate the Desired sub-structure coefficients? Do these come from the velocity of the encoder values or the velocity of the motor position for this first point? I'm really trying to figure out how the initial position, and velocity and acceleration for the trajectory is calculated when the motor was not commanded to go anywhere. I apologize if I'm asking my questions in multiple ways. I'm really trying to get as low level as possible to remove as many assumptions as possible.
-
Hi, My understanding is that the current motor velocity, acceleration, and jerk is calculated for the initial condition for a jog call. I've also gathered that these are calculated from the encoders position updates somehow so if there is encoder noise, this can throw off these calculations and send the jog off on a faster than intended trajectory. 1) Can someone tell me from what registers are the velocity, accelerations and jerk values are being calculated from? 2) A more specific question, if I change the value of the Motor[x].HomePos just before a jog is called, could this mess up the velocity, acceleration, and jerk calculations? 3) The resultant of these calculations, are they stored in the Motor[x].Desired. Trajectory Substructure Elements? Much thanks! windell
-
Thanks Charles. So for motor 0 if I want to do an absolute read of the encoder then I should pretty much set Motor[0].AbsPosSf to the same value as EncTable[0].ScaleFactor?
-
Aloha Steve, When I try the homez command, it actually zeros out the counts for that encoder. Am I doing something wrong? thanks, windell
-
Aloha, How do you do a specific absolute read? I'm sorry if this is mentioned in the manual and I haven't seen it. If so can you point me to the page? Thanks Windell
-
Forgive me for not being specific enough. We have a Power PMAC UMAC CPU with a Power UMAC rack. Do you know of any customers who have mounted a spinning drive to the Power UMAC? Other than writing to the flash card or using a USB harddrive, do you have any suggestions of how to store log files locally? thanks, f windell
-
Hi Steve, I know that this is an old thread, but I was just looking through the users manual (pg 33 of 1/6/2015 edition) and I saw that it looks like a spinning drive can be connected to the Power PMAC via SATA or PCIe. Do you have more information on how to go about doing this? Do I need to buy an additional card from DT? thanks, windell
-
Hi, I understand that this is not the deltatau recommended thing to do, but in my application, when I'm tracking a target I'm running a motion program with PVT mode and when i want to go to another target thats far away, I first stop the motion program and then I call a jog to accelerate the telescope to the next location. 1) From previous conversations, I believe that immediately after calling a jog, it will take on the current measured acceleration as measured by the encoders as opposed to taking on the command internal trajectory acceleration and propagate that forward according to Jog.Ta and Jog.Ts. Is that correct? 2) Based on your answer to #1, I would like to do a check before calling the jog to make sure that the currently measured acceleration is within certain limits. How would I go about doing this? I guess what I'm asking is that I want to poll the register that the jog uses for its initial acceleration to make sure that it is low enough before calling a jog. Again, I understand that the recommendation is to use the linear mode and never stop the motion program, but I want to try this first before making a larger change to the motion program. thanks, windell
-
Mahalo Charles I'll see if this works. thank you for the reminder about the P-variables.
-
Thanks Charles. Is it possible to do the same thing using global p-variables? I know its inefficient use of memory, but I like being able to view these variables in the scope. thanks, windell
-
Thank you Charles. As I was referring to in the OP, I'm assuming that by you suggesting the "poor man's semaphore" method that you're certain that the compile optimizer will not detect that the semaphore isn't updated from within the while loop and use Loop-invariant Code Motion resulting in a potential infinite loop. Is that correct? I just wanted to make sure because this is one caveat of someone doing their own mutex. This was my primary motivation to post here and ask before doing my own semaphore. Look at the notes under Dekker's Algorithm here and the : https://en.m.wikipedia.org/wiki/Dekker%27s_algorithm thanks, windell
-
Hi Charles, That will be a bit difficult since on the C side, I'm writing to a set of P-variables and on the script side, I am reading from the same set. So I'm not sharing any critical areas between C and script, but I am read and writing to P-variables between the two. 1) When writing to P-variables is this an atomic operation such that on the script side I won't be able to read a half modified 64-bit double? 2) How about when reading a P-variable on the script side is this an atomic operation too? 3) I'm fine with C always taking priority. However, if I set Sys.Lock[1] == 1 when I'm doing a read of the P-variables on the script side, I want to make sure that the C program will wait until the lock is released rather than overriding the lock and doing a write anyway. Can you send me an example of what you're trying? I want to compare apples to apples here. 4) How would you propose to implement a mutex for our application without using the Sys.Lock element? Please refer to below. Here is an example of what I'm doing so that were on the same page. Please note that this is greatly simplified from what were doing on our C side, I haven't checked it lately, but I'm guessing we have at least 10k lines of code. The position commands on the C side come from a host computer that is communicating with the Power PMAC. C side: Process 0: main(){ ... while(1){ pshm->P[400] = a pshm->P[401] = b pshm->P[402] = c pshm->P[403]= d usleep(1000); } ... } Process 1: Motion program side: while(1){ var1 = P400; var2 = P401; var3 = P402; var4 = P403; pvt(10); X(var1):(DEC_MOTION_VEL) X(var2):(DEC_MOTION_VEL) X(var3):(DEC_MOTION_VEL) X(var4):(DEC_MOTION_VEL) X(var5):(DEC_MOTION_VEL) }
-
Thanks Steve. I really appreciate you looking so deeply into this. I think this is a worthy reason to upgrade our firmware. In case the new firmware doesn't work, is there a repository of old firmware versions so that I can revert back to 1.5.8 if I need to? thanks, windell