Jump to content
OMRON Forums

posalux

Members
  • Posts

    5
  • Joined

  • Last visited

posalux's Achievements

Rookie

Rookie (2/14)

  • First Post
  • Week One Done
  • One Month Later
  • One Year In
  • Conversation Starter

Recent Badges

0

Reputation

  1. posalux

    Ix26

    I use the table for woodworking and as long the starting point is +/- 1mm it is OK. Thanks for the respons.
  2. posalux

    Ix26

    Hi, To use the whole table I need to put I226 on -9000000 but then it do not find the zero position of the sensor with the home command. If I put I226 on -8000000 there is no problem. Is there a limit for Ix26? peter
  3. posalux

    G-code

    Thanks ,so for the same machine it is always the same set of sub- programs ? sorry it is all new for me. So the code of the Cam program I put after the sub programs ? peter
  4. posalux

    G-code

    I have a x-y table that a use for woodworking a PMAC PC card and everthing is working with simple programs that I write myself. To use G-code (CAM program)with my card a need to translate it to pmac code. Is it necessery to add the "translation" for every program ? as far as I understand G03 jumps to program 1000 where stands do "linear " But it are always the same "translations" so can I store them on the card or so.? peter
×
×
  • Create New...