posalux
-
Posts
5 -
Joined
-
Last visited
Content Type
Profiles
Forums
Events
Downloads
Posts posted by posalux
-
-
Yes, it is -8388608 to 8388608 just like the manual says. Do you have a copy of the Turbo SRM manual?
Sorry ,yes it is in the manual .
And I will start the program with a jogging to the end of the table and do a HOMEZ.
Thanks for the quickly respons !
-
Hi,
To use the whole table I need to put I226 on -9000000 but then it do not find the zero position of the sensor with the home command.
If I put I226 on -8000000 there is no problem.
Is there a limit for Ix26?
peter
-
Thanks ,so for the same machine it is always the same set of sub- programs ? sorry it is all new for me.
So the code of the Cam program I put after the sub programs ?
peter
-
I have a x-y table that a use for woodworking a PMAC PC card and everthing is working with simple programs that I write myself.
To use G-code (CAM program)with my card a need to translate it to pmac code.
Is it necessery to add the "translation" for every program ?
as far as I understand G03 jumps to program 1000 where stands do "linear "
But it are always the same "translations" so can I store them on the card or so.?
peter
Ix26
in Pre-Turbo PMAC
Posted
I use the table for woodworking and as long the starting point is +/- 1mm it is OK.
Thanks for the respons.