Dan.Allard
Members-
Posts
23 -
Joined
-
Last visited
Content Type
Profiles
Forums
Events
Downloads
Everything posted by Dan.Allard
-
I think you want to use GetResponceFile in gplib.h. I haven't done this myself on a power pmac but I believe this is the function call you will need to use.
-
Thanks, I can look at the position feedback. I am running virtual motors that were provided for setting up web server on the PP. I just didn't know if the PP could be configured to always be on a full count. I have always worked with the turbo pmac product line in the past and don't remember ever seeing a position which wasn't configured for subcounts.
-
The motor[x].ActPos and motor[x].ActVel don't seem to be returning floating point values on my system. The motor[x].PosError is returning what I would expect. Below is what I get when I type these commands into the terminal window. Is there a setting to correct this? The software reference doesn't mention anything. motor[1].ActPos Motor[1].ActPos=5722118563 motor[1].ActVel Motor[1].ActVel=14 motor[1].PosError Motor[1].PosError=14.0083770751953125 from software refrence Motor[x].ActPos Description: Motor outer-loop feedback position Range: Floating-point Units: Motor units Motor[x].ActPos contains the present servo cycle’s net feedback position value for the outer servo loop. It is derived from the measured position in Motor[x].Pos with corrections such as those from position-table compensation and backlash compensation. It is scaled in the motor units and referenced to the power-up position. It will be subtracted from Motor[x].DesPos to obtain the following error value in Motor[x].PosError. To calculate the position relative to the motor zero position, subtract the value of Motor[x].HomePos.
-
I removed the following two lines from lighttpd.conf allowing lighttpd to run as root. This has corrected the issue and my index.cgi file will run correctly now. # change uid to (default: don't care) #server.username = "www-data" ## change uid to (default: don't care) #server.groupname = "www-data"
-
I am building a c++ gci website on a pp. When I compile and link my source code with the linking command below I can run the output program from the command line without any issues. I will see the HTML code on my screen with the correct data from the PP. however when I try to access the webpage I get the error message below about binding failed in the lighttpd error log. I quick google search got me the link below which leads me to believe that this is an issue with the group rights for www-data. But I am not sure what I need to do to add the lighttpd web server to the correct group to access the xenomai library required by libppmac. If I remove all references to the PP libraries and compile my program without linking to the PP libraries lighttpd will serve up my index.cgi webpage without any issues so the only problem I am dealing with at the moment is that lighttpd isn't able to run a program which uses the xenomai library. g++ -L /opt/ppmac/libppmac -L/usr/local/xenomai/lib -g -Wall main.o HTML_elementBase.o body.o a.o img.o -o /var/www/cgi-bin/index.cgi -l:libppmac.so \ -l:librtdk.so -l:libpthread_rt.so -l:librtdm.so -l:libxenomai.so Xenomai: binding failed: Operation not permitted. http://www.xenomai.org/pipermail/xenomai/2012-May/025831.html
-
Hi Dave, You had a good idea. I did some more research on the web and figured out the linker errors is a missing link to the exnomai library which is used by libppmac.so. There are a few shared libraries in the exnomai directory so through trial and error I determined which ones I need to get a simple program with just a library open and close function call to compile and run. the calls below from my makefile worked to produce an output file which will run. As an fyi this approach is not for the faint of heart. Several times the program compiled but something else was going off into left field when it would run until I got to the minimum list of included library files I got an error message when the program ran which which I have no idea what it meant. Until I hear otherwise I am going to assume the solution which compiles and runs must be acceptable. It would be nice to know what the error message below is all about. Also it would be good to know that just linking the libraries in with the compiler flags below is sufficient. I don't know if there are any special flags that should be used with the libraries. My hope is that any special flags would only have been needed when the libraries were compiled not at linking. My reasoning for this is simply that the linking is really just linking calls to functions with binary function code. error message which showed up when the program ran until I eliminated all the unneeded library links. Xenomai: uitron skin or CONFIG_XENO_OPT_PERVASIVE disabled. (modprobe xeno_uitron?) make: *** [default] Error 1 working makefile run make g++ -g -Wall -c -I /opt/ppmac/libppmac/ -I /opt/ppmac/rtpmac main.cpp g++ -g -Wall -c libHTML/HTML_elementBase.cpp g++ -g -Wall -c libHTML/body.cpp g++ -g -Wall -c libHTML/a.cpp g++ -g -Wall -c libHTML/img.cpp g++ -L /opt/ppmac/libppmac -L/usr/local/xenomai-2.5.6/lib -g -Wall main.o HTML_elementBase.o body.o a.o img.o -o index.cgi -l:libppmac.so -l:librtdk.so -l:libpthread_rt.so -l:librtdm.so -l:libxenomai.so
-
Just to complete the set here are the results from the /var/ftp directory. I will do some reading on the linker options and see if maybe i am missing something there. make g++ -g -Wall -c -I /var/ftp/ppmaclibs/libppmac -I /var/ftp/ppmaclibs/rtpmac main.cpp g++ -g -Wall -c libHTML/HTML_elementBase.cpp g++ -g -Wall -c libHTML/body.cpp g++ -g -Wall -c libHTML/a.cpp g++ -g -Wall -c libHTML/img.cpp g++ -g -Wall -L /var/ftp/ppmaclibs/libppmac -o index.cgi main.o HTML_elementBase.o body.o a.o img.o -l:libppmac.so /var/ftp/ppmaclibs/libppmac/libppmac.so: undefined reference to `__wrap_shm_open' /var/ftp/ppmaclibs/libppmac/libppmac.so: undefined reference to `__wrap_pthread_mutexattr_init' /var/ftp/ppmaclibs/libppmac/libppmac.so: undefined reference to `__wrap_pthread_create' /var/ftp/ppmaclibs/libppmac/libppmac.so: undefined reference to `__wrap_setsockopt' /var/ftp/ppmaclibs/libppmac/libppmac.so: undefined reference to `__wrap_bind' /var/ftp/ppmaclibs/libppmac/libppmac.so: undefined reference to `__wrap_sem_post' /var/ftp/ppmaclibs/libppmac/libppmac.so: undefined reference to `__wrap_shutdown' /var/ftp/ppmaclibs/libppmac/libppmac.so: undefined reference to `__wrap_recv' /var/ftp/ppmaclibs/libppmac/libppmac.so: undefined reference to `__wrap_ftruncate' /var/ftp/ppmaclibs/libppmac/libppmac.so: undefined reference to `__wrap_select' /var/ftp/ppmaclibs/libppmac/libppmac.so: undefined reference to `__wrap_sem_open' /var/ftp/ppmaclibs/libppmac/libppmac.so: undefined reference to `__wrap_pthread_setschedparam' /var/ftp/ppmaclibs/libppmac/libppmac.so: undefined reference to `__wrap_ioctl' /var/ftp/ppmaclibs/libppmac/libppmac.so: undefined reference to `__wrap_nanosleep' /var/ftp/ppmaclibs/libppmac/libppmac.so: undefined reference to `__wrap_sem_wait' /var/ftp/ppmaclibs/libppmac/libppmac.so: undefined reference to `__wrap_read' /var/ftp/ppmaclibs/libppmac/libppmac.so: undefined reference to `__wrap_sem_close' /var/ftp/ppmaclibs/libppmac/libppmac.so: undefined reference to `__wrap_socket' /var/ftp/ppmaclibs/libppmac/libppmac.so: undefined reference to `__wrap_pthread_mutex_unlock' /var/ftp/ppmaclibs/libppmac/libppmac.so: undefined reference to `__wrap_pthread_mutexattr_settype' /var/ftp/ppmaclibs/libppmac/libppmac.so: undefined reference to `__wrap_sem_unlink' /var/ftp/ppmaclibs/libppmac/libppmac.so: undefined reference to `__wrap_munmap' /var/ftp/ppmaclibs/libppmac/libppmac.so: undefined reference to `__wrap_pthread_mutex_lock' /var/ftp/ppmaclibs/libppmac/libppmac.so: undefined reference to `__wrap_pthread_mutex_destroy' /var/ftp/ppmaclibs/libppmac/libppmac.so: undefined reference to `__wrap_pthread_mutex_init' /var/ftp/ppmaclibs/libppmac/libppmac.so: undefined reference to `__wrap_listen' /var/ftp/ppmaclibs/libppmac/libppmac.so: undefined reference to `__wrap_pthread_mutexattr_destroy' /var/ftp/ppmaclibs/libppmac/libppmac.so: undefined reference to `__wrap_close' /var/ftp/ppmaclibs/libppmac/libppmac.so: undefined reference to `__wrap_sched_yield' /var/ftp/ppmaclibs/libppmac/libppmac.so: undefined reference to `__wrap_send' /var/ftp/ppmaclibs/libppmac/libppmac.so: undefined reference to `__wrap_mmap' /var/ftp/ppmaclibs/libppmac/libppmac.so: undefined reference to `__wrap_connect' /var/ftp/ppmaclibs/libppmac/libppmac.so: undefined reference to `__wrap_open' collect2: ld returned 1 exit status make: *** [index.cgi] Error 1
-
I tried linking to the library files in the other directory names this morning and got a very similar result but with slightly different error messages. make g++ -g -Wall -c -I /opt/ppmac/ppmac/libppmac -I /opt/ppmac/ppmac/rtpmac main.cpp g++ -g -Wall -c libHTML/HTML_elementBase.cpp g++ -g -Wall -c libHTML/body.cpp g++ -g -Wall -c libHTML/a.cpp g++ -g -Wall -c libHTML/img.cpp g++ -g -Wall -L /opt/ppmac/ppmac/libppmac -o index.cgi main.o HTML_elementBase.o body.o a.o img.o -l:libppmac.so /usr/local/xenomai/lib/libpthread_rt.so.1: undefined reference to `shm_open' /usr/local/xenomai/lib/libpthread_rt.so.1: undefined reference to `xnarch_tsc_to_ns' /usr/local/xenomai/lib/libpthread_rt.so.1: undefined reference to `xeno_fault_stack' /usr/local/xenomai/lib/libpthread_rt.so.1: undefined reference to `xeno_current_mode_key' /usr/local/xenomai/lib/libpthread_rt.so.1: undefined reference to `xeno_init_current_mode' /usr/local/xenomai/lib/libpthread_rt.so.1: undefined reference to `xeno_slow_get_current' /usr/local/xenomai/lib/libpthread_rt.so.1: undefined reference to `shm_unlink' /usr/local/xenomai/lib/libpthread_rt.so.1: undefined reference to `xeno_handle_mlock_alert' /usr/local/xenomai/lib/libpthread_rt.so.1: undefined reference to `xeno_set_current' /usr/local/xenomai/lib/libpthread_rt.so.1: undefined reference to `xeno_bind_skin_opt' /usr/local/xenomai/lib/libpthread_rt.so.1: undefined reference to `xeno_slow_get_current_mode' /usr/local/xenomai/lib/libpthread_rt.so.1: undefined reference to `xnarch_divrem_billion' /usr/local/xenomai/lib/libpthread_rt.so.1: undefined reference to `xeno_sem_heap' /usr/local/xenomai/lib/libpthread_rt.so.1: undefined reference to `__xnsig_dispatch' /usr/local/xenomai/lib/libpthread_rt.so.1: undefined reference to `xeno_sigshadow_install_once' /usr/local/xenomai/lib/libpthread_rt.so.1: undefined reference to `xeno_current_key' collect2: ld returned 1 exit status
-
I found two versions of the headers files which match but I think I have something wrong with the link to the shared library in my make files because it gives me a list of undefined reference to errors when it links. This is my first time building make files by hand. At this point I think it is a problem with the g++ command line but I can't see what is wrong. make g++ -g -Wall -c -I /opt/ppmac/libppmac -I /opt/ppmac/rtpmac main.cpp g++ -g -Wall -c libHTML/HTML_elementBase.cpp g++ -g -Wall -c libHTML/body.cpp g++ -g -Wall -c libHTML/a.cpp g++ -g -Wall -c libHTML/img.cpp g++ -g -Wall -L /opt/ppmac/libppmac -o index.cgi main.o HTML_elementBase.o body.o a.o img.o -l:libppmac.so /opt/ppmac/libppmac/libppmac.so: undefined reference to `__wrap_shm_open' /opt/ppmac/libppmac/libppmac.so: undefined reference to `__wrap_pthread_mutexattr_init' /opt/ppmac/libppmac/libppmac.so: undefined reference to `__wrap_pthread_create' /opt/ppmac/libppmac/libppmac.so: undefined reference to `__wrap_setsockopt' /opt/ppmac/libppmac/libppmac.so: undefined reference to `__wrap_bind' /opt/ppmac/libppmac/libppmac.so: undefined reference to `__wrap_sem_post' /opt/ppmac/libppmac/libppmac.so: undefined reference to `__wrap_shutdown' /opt/ppmac/libppmac/libppmac.so: undefined reference to `__wrap_recv' /opt/ppmac/libppmac/libppmac.so: undefined reference to `__wrap_ftruncate' /opt/ppmac/libppmac/libppmac.so: undefined reference to `__wrap_select' /opt/ppmac/libppmac/libppmac.so: undefined reference to `__wrap_sem_open' /opt/ppmac/libppmac/libppmac.so: undefined reference to `__wrap_pthread_setschedparam' /opt/ppmac/libppmac/libppmac.so: undefined reference to `__wrap_ioctl' /opt/ppmac/libppmac/libppmac.so: undefined reference to `__wrap_nanosleep' /opt/ppmac/libppmac/libppmac.so: undefined reference to `__wrap_sem_wait' /opt/ppmac/libppmac/libppmac.so: undefined reference to `__wrap_read' /opt/ppmac/libppmac/libppmac.so: undefined reference to `__wrap_sem_close' /opt/ppmac/libppmac/libppmac.so: undefined reference to `__wrap_socket' /opt/ppmac/libppmac/libppmac.so: undefined reference to `__wrap_pthread_mutex_unlock' /opt/ppmac/libppmac/libppmac.so: undefined reference to `__wrap_pthread_mutexattr_settype' /opt/ppmac/libppmac/libppmac.so: undefined reference to `__wrap_sem_unlink' /opt/ppmac/libppmac/libppmac.so: undefined reference to `__wrap_munmap' /opt/ppmac/libppmac/libppmac.so: undefined reference to `__wrap_pthread_mutex_lock' /opt/ppmac/libppmac/libppmac.so: undefined reference to `__wrap_pthread_mutex_destroy' /opt/ppmac/libppmac/libppmac.so: undefined reference to `__wrap_pthread_mutex_init' /opt/ppmac/libppmac/libppmac.so: undefined reference to `__wrap_listen' /opt/ppmac/libppmac/libppmac.so: undefined reference to `__wrap_pthread_mutexattr_destroy' /opt/ppmac/libppmac/libppmac.so: undefined reference to `__wrap_close' /opt/ppmac/libppmac/libppmac.so: undefined reference to `__wrap_sched_yield' /opt/ppmac/libppmac/libppmac.so: undefined reference to `__wrap_send' /opt/ppmac/libppmac/libppmac.so: undefined reference to `__wrap_mmap' /opt/ppmac/libppmac/libppmac.so: undefined reference to `__wrap_connect' /opt/ppmac/libppmac/libppmac.so: undefined reference to `__wrap_open' collect2: ld returned 1 exit status
-
I was just thinking there are a few of both header files on my system maybe I have the wrong pair? Which directory should I be linking to? 192.168.0.40:/# find -name gplib.h ./opt/ppmac/libppmac/gplib.h ./opt/ppmac/ppmac/libppmac/gplib.h ./var/ftp/ppmaclibs/libppmac/gplib.h ./.readonly/var/ftp/ppmaclibs/libppmac/gplib.h ./.readonly/var-tmpfs-mirror/ftp/ppmaclibs/libppmac/gplib.h root@192.168.0.200 192.168.0.40:/# find -name RtGpShm.h ./opt/ppmac/rtpmac/RtGpShm.h ./opt/ppmac/ppmac/rtpmac/RtGpShm.h ./var/ftp/ppmaclibs/rtpmac/RtGpShm.h ./.readonly/var/ftp/ppmaclibs/rtpmac/RtGpShm.h ./.readonly/var-tmpfs-mirror/ftp/ppmaclibs/rtpmac/RtGpShm.h root@192.168.0.200 192.168.0.40:/# find -name libppmac.so ./opt/ppmac/libppmac/libppmac.so ./opt/ppmac/ppmac/libppmac/libppmac.so ./var/ftp/ppmaclibs/libppmac/libppmac.so ./.readonly/var/ftp/ppmaclibs/libppmac/libppmac.so ./.readonly/var-tmpfs-mirror/ftp/ppmaclibs/libppmac/libppmac.so
-
Getting closer but the compiler isn't happy. It looks like I am missing another include file. I will dig into the manual and IDE help tomorrow and see what I can come up with. This is the code from main.cpp extern "C" { #include } int main(int argc, const char * argv[]) { // opens the deltatau lib InitLibrary() This is what I got when my makefile ran showing the g++ flags and the result. g++ -g -Wall -c -I /opt/ppmac/libppmac/ -I /opt/ppmac/ppmac/rtpmac/ main.cpp In file included from /opt/ppmac/ppmac/rtpmac/RtGpShm.h:2250, from /opt/ppmac/libppmac/gplib.h:31, from main.cpp:14: /opt/ppmac/libppmac/rtpmacapi.h:404: error: use of enum ‘macrocomtype’ without previous declaration /opt/ppmac/libppmac/rtpmacapi.h:457: error: use of enum ‘macrostationtype’ without previous declaration /opt/ppmac/libppmac/rtpmacapi.h:472: error: use of enum ‘macrocomtype’ without previous declaration /opt/ppmac/libppmac/rtpmacapi.h:487: error: use of enum ‘macrocomtype’ without previous declaration /opt/ppmac/libppmac/rtpmacapi.h:513: error: use of enum ‘macrocomtype’ without previous declaration /opt/ppmac/libppmac/rtpmacapi.h:530: error: use of enum ‘macrocomtype’ without previous declaration /opt/ppmac/libppmac/rtpmacapi.h:554: error: use of enum ‘macrocomtype’ without previous declaration /opt/ppmac/libppmac/rtpmacapi.h:568: error: use of enum ‘macrocomtype’ without previous declaration In file included from /opt/ppmac/libppmac/gplib.h:43, from main.cpp:14: /opt/ppmac/libppmac/cmdprocessor.h:48: error: ‘MAX_MBSOCKETS’ was not declared in this scope
-
Thanks. For some reason the files don't seem to be on the path for the g++ compiler. I had to include the full path. The extern C is because I am programming in C++. extern "C" { #include "/opt/ppmac/ppmac/libppmac/gplib.h" } There is also a typo in the other file name above it should be. /opt/ppmac/libppmac/libppmac.so
-
How do I access the gplib library from linux? I am writing a program which will run in linux and be compiled by gcc on the PP in linux. I have looked at the software reference the users manual and at the help in the IDE but I can't seem to find any reference which shows an example of programming directly in linux on the PP. I have searched the PP directory structure some and haven't found any header files. I could run gpascii in the background but I would prefer to link to a dynamic library instead. It would be more efficient than running another program in the background.
-
Is there any way to mount an external files system over ethernet with the PP? I can use sshfs to mount the DT as an external file system onto my mac but as far as i can tell the driver for SSHFS only works with fuse which requires you not be root and also require a kernel level driver. All the shared file systems I looked recently looked as though they needed kernel level support. It would be really handy for a few reasons if I could mount a filesystem on my mac from the pp. It would make a very easy way to share data out of the PP plus it would also provide a means of extending the storage space available to the pp. Right now with SSHFS I can get my mac to see the pp filesystem but i can't get the pp to see the mac filesystem.
-
I tried compiling the GCC 6.1.0 to get gain C++11 support but I am unable to get the mpfr library to compile. I set the make flag to ignore errors just to see if there are any other issues. As far as I could tell all the errors are related to that one library. When you try to compile the mpfr library there is an error in the make script something about now rule for AUTHORS which is just a text file listing the authors there is also an issue with the patches but if you make a directory patches that error will go away. the authors error I couldn't clear and I don't know make files well enough to edit it or to make a make file to replace it with. If anyone knows how to resolve this issue I would be grateful as I have a lot of C++11 code which I will otherwise have to back rev to C++98.
-
Henry I have to change the port for lighttpd to port 81. There is a program mono listening on port 80. Any idea what mono is and why it would be listening on port 80? I ask because 80 is the default http port so it would be nice to put the web server on 80 but I don't know what mono is or why it would be on port 80.
-
Thanks Henry that worked I can now use the apt get again.
-
I am a little feather along now. When I made the change listed in the other thread I was able to get it to start an update but I ended up with an error need to add sources to source.list. I found a debian source list generator below but i don't know which version of debian is the correct one to build a source list for. My concern is that i don't want to have the update try to update the kernel by mistake. https://debgen.simplylinux.ch/
-
Thanks shansen that looks like the information I need.
-
I am having some issues with apt get as mentioned in a different thread. I have a project which compiles and runs well on my Mac programmed with C++11 standard libraries. This project contains a large library which is programmed in C++11. I didn't realize the gcc compiler on the PP doesn't support C++11 but only the older C++0x standards. Is it safe to upgrade to the newer compiler? I don't know what effect this might have on the pp. My concern is that it might affect how the IDE compiles code. The project I am working on involves accessing information in the PP for example the motor position and posting it to a webpage. I have a C++11 html class library I am trying to use with the pp. Below is the version of the PP I am using as reported at login. I am wondering if there are some updates which might resolve the issues i am dealing with. Linux powerpmac 2.6.30.3 #34 Tue Dec 17 09:52:34 PST 2013 ppc --------------------------------- -- PowerPMAC Motion Controller -- ---------------------------------
-
I think this forum link below is the same problem I am seeing. I don't know how I would go about changing the update source as it suggest in the link below or if it is a good idea. http://forums.debian.net/viewtopic.php?f=30&t=78447 Here is the output from my apt-get update it looks to be the same issue discussed in the link above. 192.168.0.21:/opt/ppmac# apt-get update Ign http://security.debian.org lenny/updates Release.gpg Ign http://security.debian.org lenny/updates/main Translation-en_US Ign http://security.debian.org lenny/updates Release Ign http://security.debian.org lenny/updates/main Packages/DiffIndex Ign http://security.debian.org lenny/updates/main Sources/DiffIndex Err http://mirror.anl.gov lenny Release.gpg Could not resolve 'mirror.anl.gov' Err http://mirror.anl.gov lenny/main Translation-en_US Could not resolve 'mirror.anl.gov' Ign http://security.debian.org lenny/updates/main Packages Ign http://security.debian.org lenny/updates/main Sources Ign http://security.debian.org lenny/updates/main Packages Ign http://security.debian.org lenny/updates/main Sources Err http://security.debian.org lenny/updates/main Packages 404 Not Found [iP: 128.31.0.63 80] Err http://security.debian.org lenny/updates/main Sources 404 Not Found [iP: 128.31.0.63 80] Ign http://volatile.debian.org lenny/volatile Release.gpg Ign http://volatile.debian.org lenny/volatile/main Translation-en_US Ign http://volatile.debian.org lenny/volatile Release Ign http://volatile.debian.org lenny/volatile/main Packages/DiffIndex Ign http://volatile.debian.org lenny/volatile/main Sources/DiffIndex Ign http://volatile.debian.org lenny/volatile/main Packages Ign http://volatile.debian.org lenny/volatile/main Sources Ign http://volatile.debian.org lenny/volatile/main Packages Ign http://volatile.debian.org lenny/volatile/main Sources Err http://volatile.debian.org lenny/volatile/main Packages 301 Moved Permanently [iP: 130.89.148.14 80] Err http://volatile.debian.org lenny/volatile/main Sources 301 Moved Permanently [iP: 130.89.148.14 80] Reading package lists... Done W: Failed to fetch http://mirror.anl.gov/debian/dists/lenny/Release.gpg Could not resolve 'mirror.anl.gov' W: Failed to fetch http://mirror.anl.gov/debian/dists/lenny/main/i18n/Translation-en_US.bz2 Could not resolve 'mirror.anl.gov' W: Failed to fetch http://security.debian.org/dists/lenny/updates/main/binary-powerpc/Packages 404 Not Found [iP: 128.31.0.63 80] W: Failed to fetch http://security.debian.org/dists/lenny/updates/main/source/Sources 404 Not Found [iP: 128.31.0.63 80] W: Failed to fetch http://volatile.debian.org/debian-volatile/dists/lenny/volatile/main/binary-powerpc/Packages 301 Moved Permanently [iP: 130.89.148.14 80] W: Failed to fetch http://volatile.debian.org/debian-volatile/dists/lenny/volatile/main/source/Sources 301 Moved Permanently [iP: 130.89.148.14 80] W: Some index files failed to download, they have been ignored, or old ones used instead. W: You may want to run apt-get update to correct these problems root@192.168.0.200
-
I found a workaround to this but figured it was worth mentioning. I tried to add a user to linux on my pp. I figured it would be nice not to have to work as root and the ftp connection was refused as root by the pp. Anyway adding the user account was easy enough and the ftp was working good. But when the pp was power cycled the user account was removed. The home directory for my user was still there but the user account was not listed in the password file. My solution has been to use sshfs to transfer my files instead of ftp because sshfs doesn't care if you use root and it is actually easier to use with mac osx then fetch and ftp. But it would be nice to be able to add a user and not have to work as root in linux.
-
I am trying to setup lighttpd on a power pmac. I have the power pmac connected to the web through a DNS server and I can ping www.google.com successfully from the pp. When I try to do an apt-get update or apt-get build-dep lighttpd I get a long list of error messages about not being able to resolve the mirror.anl.gov sample error message. Err http://mirror.anl.gov lenny/main libglib2.0-0 2.16.6-2 Could not resolve 'mirror.anl.gov' I have tried pinging this server from my mac as well as the pp and I am unable to reach it from either machine. I have the source code for lighttpd but when i try to run the configuration program it give me the following error configure: error: pcre-config not found, install the pcre-devel package or build with --without-pcre I am in the process of setting up lighttpd to host a cgi webpage programmed in C++ so I could probably compile without pcre as it is related to pearl but i would like to build it with pearl support.