Jump to content
OMRON Forums

Bhagesh

Members
  • Posts

    4
  • Joined

  • Last visited

Recent Profile Visitors

The recent visitors block is disabled and is not being shown to other users.

Bhagesh's Achievements

Rookie

Rookie (2/14)

  • First Post
  • Week One Done
  • One Month Later
  • One Year In
  • Conversation Starter

Recent Badges

0

Reputation

  1. Dear Sir, We have CK3M ETHERCAT CPU-111 + AX1515n + MD7110 + MD7120 installed for a 6 axis Reshrpening Machine. 5 servo's are of Delta ASDA-A2-E 1Khz Ethercat and 1 VFD for Spindle. we are facing certain problems in configuring and using the setup which are as follows. the PC config is Advantek Indl. core I7 CPU with 8gb ram and 1th SSD. with win 64bit OS. 1) Power Pmac IDE 4.3 hangs frequently after configuring and Tuning delta asda-a2-e EtherCat Motors on Windows 8.1 pro and win 7 64bit. Kindly suggest proper system cpu frequency settings. currently we used 4khz phase and 1khz servo freq, 2) initially first AX1515N unit became faulty due to some component got burnt. hence we replaced it with a new one. after the whole stsyem was setup and we were uploading PLC and Motion profiles. 3) suddenly since yesterday, CK3M cpu has stopped detecting any hardware like AX1515n + MD7110 + MD7120, though the Ethercat acountis master is working but hangs after 15-20 mins of use. 3) we are not able to set diff phase freq. and its automatically sets similar as the servo freq. 1khz. by default.. tried "$$$***" to reset to factory default but it wont help. 4) currently Ck3m CPU is only detecting Ethercat Master and do not recognises the remaining hardware attached to it. attahced herewith some pics to explain the cou details and current condition. will replacing or upgrading the firmware can help??? kindly send your suggestions. Bhagesh Lokhande.
  2. hII, I HAVE CK3M ETHERCAT CPU +AX1515n+MD7110+MD7120 , AFTER ALL WIRING WAS DONE AND ALL 4 AXIS FROM AX1515N AND MD7110 AND MD7120 I/O'S WERE WORKING OK N FINE. TODAY AFTER POWERING UP THE 4 AXIS FRON AX1515N STOPPED WORKING. IDE SHOW SYS.NOCLOCKS ALARAM. YET MD7110 AND MD7120 ARE WORKING FINE. KINDLY ADVICE FOR FURTHER TROUBLESHOOTING.
  3. hii everyone, i am using Geobrick Turbopmac2 4 axis, and need to move tool on precise Gear Involute profile Path using Rotary Axis (c ) and Radial Axis (Y). Need to know if there is any Involute Interpolation available. Y Axis Position = R(Theta)sin(Theta) C Axis Position = Tan(Theta)-Theta where (Theta) is the Roll Angle of the Gear in Radians with ® as the Base Circle Radius of the Gear. Thanks & Regards B.J.
  4. I am using CEM Clipper Turbo PMAC2-Eth-Lite 4 axis flag board which i bought from korea, using it for 4 stepper axis , one linear feedback scale on JHW handwheel port, 2 analog in ports for LVDT, and want to use 16 digital Inputs and 12 Digital Outputs from JOPTO port and JTHW Multiplexer Ports, All 4 axis with stepper motors along with their Limitswitches are working fine, Analog Inputs are also working ok, I am also to get the Scale feedback from the handwheel encoder port, But i am facing difficulties in accessing the Digital Inputs and outputs Through JTHW Multiplexer Port, Need proper M variable defs for the same, and also not able to get the referencing of the Linear Scale Feedback through JHW Port. Can you Kindly guide me for the same???? Thanks and Regards,
×
×
  • Create New...