dhidas
-
Posts
4 -
Joined
-
Last visited
Content Type
Profiles
Forums
Events
Downloads
Posts posted by dhidas
-
-
I'm looking to use it in a PLC (script language)
-
I'd like to have a shorthand way to look at the bits in SerialEncDataB, for example looking at the CRC bit etc. I thought something like this might work, but it doesn't seem to. Is there a good way to do this without having to do all of the bit shifting in a PLC?
#define LENC1CRC Acc84E[0].Chan[0].SerialEncDataB.22.1
-
Hello,
I am using direct microstepping on #1 of a GeoBrick LV and wish to use the position compare functionality as a trigger of sorts (in this case step as there is no encoder). I setup #5 as a virtual motor following the instructions for PFM so that I could use the position compare on #5 when it is following #1. The problem I am currently having is that #5 lags significantly behind #1 at higher speeds. I tried setting program acceleration and velocity to high values, the s-curve and accl-times to very small values for #5, and upped the PFM frequency, but I see no change in the amount of following error. Is there any other way to make #5 more synchronized with #1?
Thanks for your help,
-Dean
SerialEncDataB Acc84E bits
in Power PMAC
Posted
Thanks, this looks to be what I was after!
(small correction is a missing : after u.user): ptr LENC1CRC->u.user:$3000.4.1