mao
-
Posts
3 -
Joined
-
Last visited
Content Type
Profiles
Forums
Events
Downloads
Posts posted by mao
-
-
Thanks for you reply.That what I want exactly.
So you pmac works in the close loop mode,I mean you get the feedback data from profibus.
How many axis you control throw the profibus?
2ms was too slow for close loop control I think,can I control that using open loop way?I mean only send position command to servo drive throw profibus,the only question worried me was the precision of the position command,24bits? or higher?
hello, how are you use 72e control drive with open loop way ?
-
Power UMAC use Linux . does Power UMAC can read USB device? and how to do? The device can run on c++
velocity limit in spline mode
in Turbo PMAC
Posted
hi all;
I used spline2 mode in prog;
this is my code:
#define Motor11Pos P1000
#11->X;
open prog 1 CLEAR
I42 =0;
SPLINE 2 TM20;
abs;
WHILE(Start_flag=1)
X(Motor11Pos);
ENDW
close
Now, the P1000 is dynamic and ruleless! so I want to limit max velocity of #11 .
the parameter Ixx16 no works to limit motor velocity.
how can i do to limit ?
thanks .