Jump to content
OMRON Forums

New IDE installation fails.


JeffLowe

Recommended Posts

  • Replies 7
  • Created
  • Last Reply

Top Posters In This Topic

You can also look at the log we create in installtion. The location... \Program Files\Delta Tau Data Systems Inc\2.0\Power PMAC Suite\ConfigFiles\Deltatau_Installation.log When do you get the error in the begining or in the middle ? I will need more information about the error so I can help. Atul [quote='JeffLowe' pid='1250' dateline='1296569630'] Power PMAC Suite Installshield Wizard X CreateFile failed OK Closes... [/quote]
Link to comment
Share on other sites

[quote='agovande' pid='1256' dateline='1296579486'] You can also look at the log we create in installtion. The location... \Program Files\Delta Tau Data Systems Inc\2.0\Power PMAC Suite\ConfigFiles\Deltatau_Installation.log When do you get the error in the begining or in the middle ? I will need more information about the error so I can help. [/quote] c:\Program Files\Delta Tau Data Systems inc exists but there is nothing stored under that, no 2.0 or any other subdirectories.
Link to comment
Share on other sites

[quote='JeffLowe' pid='1258' dateline='1296581974'] [quote='agovande' pid='1256' dateline='1296579486'] You can also look at the log we create in installtion. The location... \Program Files\Delta Tau Data Systems Inc\2.0\Power PMAC Suite\ConfigFiles\Deltatau_Installation.log When do you get the error in the begining or in the middle ? I will need more information about the error so I can help. [/quote] c:\Program Files\Delta Tau Data Systems inc exists but there is nothing stored under that, no 2.0 or any other subdirectories. [/quote] I've got past a similar problem by renaming (to hide them) the installShield cache in Program\ Files/InstallShield\ Installation\ Information. Possibly a bit drastic but perhaps will help identify the problem. -adrian
Link to comment
Share on other sites

In trying to get my project to build again under the new IDE, I'm consistently getting this error in pp_error.log. I also have an empty pp_proj.h file; could this be why ? 2 [main] projpp 3068 _cygtls::handle_exceptions: Exception: STATUS_ACCESS_VIOLATION 15948 [main] projpp 3068 open_stackdumpfile: Dumping stack trace to projpp.exe.stackdump The stackdump contains : Exception: STATUS_ACCESS_VIOLATION at eip=004060F2 eax=00000000 ebx=00000000 ecx=00000000 edx=0022A004 esi=611021A0 edi=0040CF90 ebp=0022A038 esp=0022A010 program=C:\Program Files\Delta Tau Data Systems Inc\2.0\Power PMAC Suite\powerpc-460-linux-gnu\bin\projpp.exe, pid 3068, thread main cs=001B ds=0023 es=0023 fs=003B gs=0000 ss=0023 Stack trace: Frame Function Args 0022A038 004060F2 (00000000, 0022A7A0, 00010000, 0022A074) 0022AFC8 00402732 (0022C450, 006827D4, 0068269C, 0068276C) 0022CC88 00401D3D (0040F940, 0040E37C, 0040E32D, 0040FF10) 0022CCC8 004013C0 (00000001, 00682650, 00680090, 61010E8C) 0022CD98 610060D8 (00000000, 0022CDD0, 61005450, 0022CDD0) 61005450 61004416 (0000009C, A02404C7, E8611021, FFFFFF48) 827969 [main] projpp 3068 _cygtls::handle_exceptions: Exception: STATUS_ACCESS_VIOLATION 853029 [main] projpp 3068 _cygtls::handle_exceptions: Error while dumping state (probably corrupted stack) Furthermore, if I work around the problems this creates in the build process and continue to download, I get Projpp Error Projpp has exited with : Segmentation fault root@192.168.0.200:/opt/ppmac# Download process failed with a segmentation fault. Which is apparently the same utility failing in the Linux environment. -adrian
Link to comment
Share on other sites

[quote='artag' pid='1260' dateline='1296603100'] I've got past a similar problem by renaming (to hide them) the installShield cache in Program\ Files/InstallShield\ Installation\ Information. Possibly a bit drastic but perhaps will help identify the problem. [/quote] This worked, but rather than hiding the whole InstallShield directory, I simply deleted the B9A0C1FA-E2D2-431F-A151-B932B5CC191C subfolder.
Link to comment
Share on other sites

in Win7 64 bit the directory to delete in the Program Files\InstallShield (x86) directory is: {ACB3690A-F2AB-4504-9ED1-8957FAB61CAC}
Link to comment
Share on other sites

Guest
This topic is now closed to further replies.

×
×
  • Create New...