Jump to content
OMRON Forums

Recommended Posts

Posted

Hi,

can someone please help me with how to set the variable Ix22 (in PEWIN) in order to change the jog speed of motor x?

In PEWIN I tried "I122=2000" to change the jog speed of motor 1 to 2000 counts/msec (as on-line command). However the value of I122 did not change. In PEWIN it looks like that:

I122

3500

I122=2000

I122

3500

According to the TYPE command, I'm using a PMAC Turbo2. PEWIN gives me that:

TYPE

Turbo2, X8

Another variable of interest could be I50. PEWIN gives me that:

I50

20

By the way, changing the homing speed by setting variable Ix23 works.

Thank you for your help!

 

  • Replies 6
  • Created
  • Last Reply

Top Posters In This Topic

Posted
Do you have any PLCs running that might be resetting the value of Ixx22? Perhaps you could disable all PLCs temporarily (CTRL+D or I5=0) and try setting the value again. If this does not work, please call our Technical Support Hotline and we can try to troubleshoot over the phone -- (818) 717-5656, 8 am-5 pm PST.
Posted

Thank you very much CharlesP!

After setting I5 to 0, I was able to change the jog speed of the motors. Setting it back to its former value I5=0 automatically resets Ix22 to its former value.

 

Posted

No I haven't, yet. However, it's a program generated by NCUI. Is there a possibility to access the PMAC program that NCUI sends to PMAC?

 

 

Posted
Note that the NCUI standard control panel PLC will override the Ix22 setting. This is used in the "Manual" mode for jogging the axes. If you disable the control panel PLC you should have control of the Ix22.
Guest
This topic is now closed to further replies.

×
×
  • Create New...