hongchinlin_992x Posted April 12, 2011 Share Posted April 12, 2011 I have three ACC-72E cards with me. One of them is supposed to be a Profibus card, while the other two are CAN cards. However, they all look the same. How to tell one from the other? Link to comment Share on other sites More sharing options...
Sina.Sattari Posted April 12, 2011 Share Posted April 12, 2011 ACC-72E uses different Hilscher modules for different protocols. Here is a list of Hilscher modules which are being used on ACC-72E: Module Fieldbus ----------- ----------------- COM-DPM Profibus Master COM-DPS Profibus Slave COM-CA-DNM DeviceNet Master COM-CA-DNS DeviceNet Slave COM-COM CanOpen Master COM-COS CanOpen Slave COM-CNS ControlNet Slave COM-CN-CCS CC-Link Slave Link to comment Share on other sites More sharing options...
hongchinlin_992x Posted April 12, 2011 Author Share Posted April 12, 2011 The two cards (COM-DPM and COM-COM) phyaically are identical. There is no marking for differentiation, at least not from the visible side. Link to comment Share on other sites More sharing options...
pennells Posted June 24, 2011 Share Posted June 24, 2011 ACC-72E uses different Hilscher modules for different protocols. Here is a list of Hilscher modules which are being used on ACC-72E: Module Fieldbus ----------- ----------------- COM-DPM Profibus Master COM-DPS Profibus Slave COM-CA-DNM DeviceNet Master COM-CA-DNS DeviceNet Slave COM-COM CanOpen Master COM-COS CanOpen Slave COM-CNS ControlNet Slave COM-CN-CCS CC-Link Slave Can any of the CanOpen versions be used to run raw CanBus communications or does the CanOpen layer have to be included? Link to comment Share on other sites More sharing options...
Sina.Sattari Posted June 24, 2011 Share Posted June 24, 2011 pennells, We use Hilscher modules for these boards. The memory on these modules act as a Dual Ported RAM to PMAC and all the other communication requirements are done by Hilscher module. If you need detailed information, you need to contact Hilscher. Regards, Link to comment Share on other sites More sharing options...
Recommended Posts