Jump to content
OMRON Forums

ABS mode with X and Y axes


franz91
 Share

Recommended Posts

  • Replies 4
  • Created
  • Last Reply

Top Posters In This Topic

Top Posters In This Topic

Hi,

 

I have a system with motor #1 which control X and Y axis and motor #2 which control Y axis.

The coordinate system is : #1-> 8000X and #2-> -8000X+8000Y

But I want control my system as a rotation system, like it is possible with A and B (I want command my axis as angles and roll-over when I want).

But as it was already said I can't make a CS like #1-> 8000A and #2->-8000A+8000B.

 

With #1-> 8000X and #2-> -8000X+8000Y, when I ask, at home position, in a motion program, X(370), it's make a complete round plus 10 degrees, but I want the shortest move (a move of -10 degrees in this example, like when I command A(370) with roll-over enabled).

Link to comment
Share on other sites

If you want to do custom axis definitions that PMAC normally does not allow or understand, you can just define your motors to use kinematics as such:

 

&1 
#1->I
#2->I

 

Then you can configure whatever relationship between motor and axis that you want in your kinematics subroutines.

 

Please refer to the Power PMAC Coordinate Systems manual, Coordinate-System Kinematic Subroutines section (page 8 and following on latest version) for more information on setting up kinematics.

Link to comment
Share on other sites

Guest
This topic is now closed to further replies.
 Share


×
×
  • Create New...