JohnR Posted May 19, 2011 Share Posted May 19, 2011 What is the recomended method for sharing the motor/amplifier database ? I would like to have a master database that gets appended to for each system that we build and used that same database as we move forward. Can the database be on a network drive ? How do I transfer the complete database to multiple systems ? Is there a Delta Tau database with common motor/amplifiers already defned ? Thanks John Link to comment Share on other sites More sharing options...
Sina.Sattari Posted May 19, 2011 Share Posted May 19, 2011 John, The System Setup software for Power PMAC, comes with preloaded with all supported Delta Tau amplifiers (we will add Brick family later once we have a Power Brick product and will add Geo MACRO once we have MACRO support). There are 2 other custom databases which are designed to hold your motor and amplifier data for future use on the same PC which they are entered. These 2 databases can be exported/imported from/to other PCs which have Power PMAC IDE installed. At the moment, there is no automatic support for updating a centralized database and has to be done manually. Although it's a nice suggestion, we (Delta Tau Data Systems, Inc.) will not be able to play host for this centralized database since we don't have a way to authenticate correct data submission by users. However, we MIGHT be able to do something if you want to define a SQL server or MySQL server to hold the data for your organization. Regards, Link to comment Share on other sites More sharing options...
Recommended Posts